2024-10-02 2:12 PM
Hi:
I have a code written with ST Cube IDE 1.6.1.
I need to add a new characteristic, but with the latest version (1.16.1), the code doesn't compile well.
On this link there is an option to download older versions:
https://www.st.com/en/development-tools/stm32cubeide.html
but it is impossible to download the version that I need.
After this screen, nothing happens.
Is it possible to send me a link via email to download it ?
Regards
2024-10-03 7:38 AM
Hello @j_rios and welcome to ST Community,
>> the code doesn't compile well.
It's recommended to use the latest version of Tools which contains enhancement and bug fixes.
What kind of issue do you observed? What exactly did the error message say?
Perhaps the setting of your project is not set up properly?
2024-10-03 7:53 AM
However, I share with you the version of STM32CubeIDE (v1.1.6) you need, to find a way out of that situation.