2019-06-03 11:27 AM
When I firsts Installed the STM32Cube IDE got all kind of error in paths and other stuff, so tried to uninstall it, the uinstallation was always freezing and I deleted the folders. Also, tried to delete some registers but could not find anything more..
So, when I try to install it again, I get this message.
What should I do to force it to install?
Also, I ve Atollic 9.3.0 installed and my current project is beeing developed on it.
2019-06-04 5:42 AM
Ethan Huang gave a great answer to this which I will just paste here:
2020-03-31 12:52 PM
Hello
Sorry if I intervene in this answer, but I have a similar question.
If I want to uninstall an old version of STM32cubeIDE on Linux (Ubuntu) what should I do?
Is there an uninstall file ?
Do I have to brutally delete the following directors ?
/ opt / st
/ Home / "users" / STM32Cube
/ Home / "users" / STM32CubeIDE
Thanks for the reply
Hal
2021-07-28 1:08 PM
dpkg --remove --force-remove-reinstreq st-stm32cubeide-1.6.1
2022-05-31 9:02 PM
In case someone deleted the /opt/st folder (Ubuntu), And the installer says there is "nothing to install":
"UM2563 STM32CubeIDE installation guide" says to run this command:
The uninstallation of STM32CubeIDE depends on the distribution. Uninstall STM32CubeIDE according to the step
below corresponding to the distribution used:
...
• For Debian-based distributions (such as Debian®, Ubuntu® or others):
sudo apt-get remove st-stm32cubeide-xxxx st-stlink-udev-rules st-stlink-server segger-jlink-udev-rules
But for me this one worked:
sudo apt-get remove st-stlink-udev-rules st-stlink-server segger-jlink-udev-rules
I just installed Xubuntu 22.04 and Initially STM32CubeIDE froze right after being installed. It did nothing but hover over a menu and nothing could be clicked, nothing could be triggered, not even a terminal window. Had to force shutdown manually on the power button. After that the IDE could no longer be initialized. I found something on the Internet about a .lock file in the WorkSpace folder, but it didn't do anything to remove that file.
It would be nice if the installer could check what's missing, like the /opt/st folder instead of just saying there's nothing to install.