cancel
Showing results for 
Search instead for 
Did you mean: 

How to include a downloaded library into STM32CubeIDE?

DocAlex
Associate II

Hello,

 

I have downloaded a library containing two files: the .h file and the .c  file:

 

Lib.png

I used drag and drop and dropped the folder into the driver folder of my project. I selected them to be a reference and a relative path.

includeProblem.png

 

Then I selected the compiler include path:

 

includeProblem2.png

 and the linker path

includeProblem4.png

The IDE is showing the resource correctly linked to the project:

includeProblem3.png

 when I build the project I still get the error message:

includeProblem0.png

 

What is wrong with my approach?

How do I set the paths correctly?

As a suggestion: I have found many users struggling with this. I would like to recommend a dialog for dropping a folder into the project with predefined links to the new folder.

Regards

 

Alexander

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

It's in "<project>/Drivers/Si7021". Your paths assume it's in "<project>/Si7021".

TDK_0-1745862059709.png

 

To keep consistency, you could add "../Drivers/Si7021" as the path.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
TDK
Guru

It's in "<project>/Drivers/Si7021". Your paths assume it's in "<project>/Si7021".

TDK_0-1745862059709.png

 

To keep consistency, you could add "../Drivers/Si7021" as the path.

If you feel a post has answered your question, please click "Accept as Solution".
Pavel A.
Evangelist III

Unfortunately Eclipse is too complicated for beginners. 

What you want here is "Build variables", not "linked resources".

Also, what you call a library is just an additional source file for the purpose of the project. So you don't add it to the libraries & library search path. Libraries are ".a" files.

 

Thank you very much!

Another issue was that I had an include "-l" which was expecting an archive.

Regards

 

Alexander