2024-12-10 11:18 AM
1. Which CubeIDE version is the latest that supports MacOS 12.7 Monterey for the Intel-based Macs?
2. Where do I go to download it?
Thanks
2024-12-11 12:21 AM - edited 2024-12-11 4:22 AM
Hello @noName123
I recommend using the latest STM32CubeIDE 1.17.0, which supports the following operating systems and architectures:
Please note that while STM32CubeIDE may work on macOS 12.7, it is not officially supported on this version. Therefore, to ensure proper functionality on macOS 12.7, I recommend using a virtual machine (VM) with one of the supported operating systems listed above.
You can download the latest STM32CubeIDE from this LINK
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-12 7:55 AM
Thank you for your reply.
Do any earlier versions of CubeIDE support MacOS 12.7?
I've had bad experience using a virtual machine with other tools and would rather use an earlier version of CubeIDE if there is one that supports my OS.