2022-09-08 1:58 AM
I am New to the STM32H723Z controller. I want to enable and disable the JTAG-DP pins temporarily by using code. Any sample code or clue appreciated .
2022-09-12 1:32 AM
Hello @SSaid.1
You just have to reprogram the GPIO pins via GPIO_Init().
Or uses the LL as i do to restore the SWD functionality in case of Error :
#define GPIO_SW_PORT GPIOA
#define GPIO_SWDIO_PIN LL_GPIO_PIN_13
#define GPIO_SWCLK_PIN LL_GPIO_PIN_14
__HAL_RCC_GPIOA_CLK_ENABLE();
LL_GPIO_SetPinPull(GPIO_SW_PORT, GPIO_SWCLK_PIN, LL_GPIO_PULL_DOWN);
LL_GPIO_SetAFPin_0_7(GPIO_SW_PORT, GPIO_SWCLK_PIN, LL_GPIO_AF_0);
LL_GPIO_SetPinMode(GPIO_SW_PORT, GPIO_SWCLK_PIN, LL_GPIO_MODE_ALTERNATE);
LL_GPIO_SetPinPull(GPIO_SW_PORT, GPIO_SWDIO_PIN, LL_GPIO_PULL_UP);
LL_GPIO_SetAFPin_0_7(GPIO_SW_PORT, GPIO_SWDIO_PIN, LL_GPIO_AF_0);
LL_GPIO_SetPinMode(GPIO_SW_PORT, GPIO_SWDIO_PIN, LL_GPIO_MODE_ALTERNATE);
BR,
Bruno
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.