cancel
Showing results for 
Search instead for 
Did you mean: 

How do you add a .ioc file to an existing project that does not have one?

KiptonM
Lead

I got the example files from here:

You are missing the famous set of examples for UART with DMA by Tilen Majerle.

https://github.com/MaJerle/stm32-usart-uart-dma-rx-tx

I selected the project usart_dma_rx_idle_line_irq_F4.

First thing I notice, it did not have a .ioc file for me to configure the rest of the chip.

I do not know how to fix this. It is for a generic F4. I have a Nucleo-F446RE.

Is the missing .ioc the cause of the error:

arm-none-eabi-objcopy.exe -O ihex "usart_dma_rx_idle_line_irq_F4.elf" "usart_dma_rx_idle_line_irq_F4.hex"

/bin/sh: 1: arm-none-eabi-objcopy.exe: not found

make[1]: *** [makefile:84: post-build] Error 127

make: *** [makefile:52: all] Error 2

"make -j12 all" terminated with exit code 2. Build might be incomplete.

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
KiptonM
Lead

I scrwed up the file, and decided it was best to re-download the project.

I looked over the projects and wanted to have an example with transmit DMA. The Documentation said:

Examples for RX & TX

  • Available in projects folder with usart_tx_prefix
  • DMA is used to receive data and to transmit data back
  • It uses ring buffer to copy data from DMA buffer to application buffer first

Unfortunately there were no examples that started with usart_tx. There were only usart_rx.

I wanted to see if I could get something to work. Since I have a Nucleo-F446RE there were only 2 choices.

usart_rx_idle_line_irq_F4

usart_rx_idle_line_irq_rtos_F4

And since I did not want RTOS I went with usart_rx_idle_line_irq_F4

I used File->Open Projects from File System, and pointed into that directory (/home/kip/STM32CubeIDE/stm32-usart-uart-dma-rx-tx-master/projects/usart_rx_idle_line_irq_rtos_F4)

Deleted the post build command with arm-none-eabi-objcopy.exe program. I have searched the whole computer and did not find the file. )

Compiled Project with no errors or warnings.

I put my FTDI TTL-232R-3V3-WE cable on the USART3 TX and RX and Gnd. Set up the moserial program to look at the the /dev/ttyUSB0 and set it at 115200 Baud 8-N-1 No handshake.

And started in the debugger. It appears it went directly to HardFault_Handler(void) in the stm32f4xx_it.c file. And then stayed in the empty while(1) loop.

Maybe the program does not like the debugger.

So I ran it. Since I have never just ran a program not sure how it is supposed to go but it said

Download verified successfully

Debugger connection lost.

Shutting down...

Which I am guessing is correct.

And nothing happens. I tried typing something to see if it echoed back. Nothing.

So I am guessing something is wrong an it is in the same Hard_Fault_Handler() it went to in the Debugger.

What should I do next?

KiptonM
Lead

By the way I know my serial ports are working because I have another program that does a simple polling write to each serial port

/* USER CODE BEGIN 0 */

uint8_t data1[] = {"11111111111111111111111111111111111111111111111111111111111111\r\n"};

uint8_t data2[] = {"22222222222222222222222222222222222222222222222222222222222222\r\n"};

uint8_t data3[] = {"33333333333333333333333333333333333333333333333333333333333333\r\n"};

uint8_t data4[] = {"44444444444444444444444444444444444444444444444444444444444444\r\n"};

uint8_t data5[] = {"55555555555555555555555555555555555555555555555555555555555555\r\n"};

uint8_t data6[] = {"66666666666666666666666666666666666666666666666666666666666666\r\n"};

/* USER CODE END 0 */

And then farther down it has

 while (1)

 {

   /* USER CODE END WHILE */

   /* USER CODE BEGIN 3 */

    HAL_UART_Transmit(&huart1, data1, sizeof(data1), 1000);

    HAL_UART_Transmit(&huart2, data2, sizeof(data2), 1000);

    HAL_UART_Transmit(&huart3, data3, sizeof(data3), 1000);

    HAL_UART_Transmit(&huart4, data4, sizeof(data4), 1000);

    HAL_UART_Transmit(&huart5, data5, sizeof(data5), 1000);

    HAL_UART_Transmit(&huart6, data6, sizeof(data6), 1000);

    HAL_Delay(250);

 }

 /* USER CODE END 3 */

And that works on all the ports except USART2. I now have had 2 boards where USART2 does not work. the other 5 do. But that is another issue.