2021-08-16 5:57 AM
Hi, i have added remote connection in STM32CubeIDE (preferences > Remote development > Remote connections)
Now i need to modify the project present in the folder of remote connection
How can i modify the project present in remote PC connection
2021-08-17 5:47 AM
Hello there!
What are you trying to modify? How the project presents itself to the screen? Is there information that is missing?
Could you add a screenshot to the thread of how it looks and what you would like to modify?
2021-08-23 4:02 AM
Hi @Markus GIRDLAND
Sorry for the delay in replay
Actually iam using stm32mp1 processor , so i want to modify the example M4 projects using STM32CUbeIDE which are present in linux Distribution package .
which is present in linux virtual machine which i can access only using SSH.
so i have created remote connection in STM32Cube IDE ,iam able to access the console of remote connection but iam unable to find any directory in project explorer.
FYI : the projects already present in project explorer are not from the virtual machine
2021-08-24 8:16 AM
Hi Maksh.1,
To clarify about M4 projects:
. Starter kit provides you with SDCard content which includes M4 binaries:
. they appears on the target under /usr/local/Cube-M4-examples
. you can access them via Linux console
. inside STM32CubeIDE you can import those examples from STM32CubeFirmware,
. they will appear inside Project Explorer of STM32CubeIDE
. you can compile them, and debug them. In case of debug in production mode, M4 binary is donwloaded on the target /usr/local/projects/<prj_name>/ ...
To have a better idea of STM32CubeIDE purpose I recommend you to have a look to https://wiki.st.com/stm32mpu/wiki/STM32CubeIDE
Hope this help,
LudovicR
2021-08-26 2:09 AM
Thanks @LudovicR
my requirement is i have a remote linux PC which i can access only through ssh ,
Now my question is how can i import the M4 project example present in Distribution package which present in Linux PC and modify it using Cube IDE .
after modifying it i need to build linux image along with the m4 project in linux PC without copying and pasting the M4 example in Distribution package.