2024-01-03 10:49 PM - edited 2024-01-03 10:51 PM
Hi,
I have a simple question. I'm using STM32CubeIDE v1.14.0 on MacOS and I want to use Doxygen for the source code documentation. The problem is that the shortcut for Login to myST is the same as the "@" shortcut. So it is not possible to write the "@", because every time the login popup comes up.
Does anybody knows how to disable the login shortcut (OPTION+L)?
2024-01-04 5:37 AM
I can see that it's a known issue, because the shortcut is hard coded and cannot be disabled or changed at the moment.