2023-06-04 5:41 AM
2023-06-04 6:00 AM - edited 2023-11-20 4:03 AM
Hello
Check in the project -> properties output formats you need:
2023-06-04 7:15 AM
I thought STM32 Cube Programmer supported .ELF in the writing tab? ST-LINK Utilities is deprecated for MANY YEARS
Add post-build to convert to .BIN (files) or . HEX
.BIN singular can be problematic if image is sparse, describing regions GB apart.
2023-06-04 7:17 AM
Thank you JTP. Today is Sunday and you're ready to answer.
Best regards, Ilson
2023-06-04 7:25 AM
Thank you again DeLorean. I'm waiting a answer for tomorrow!!! Aujoud'hui est Dimanche.
Best regards, Ilson