cancel
Showing results for 
Search instead for 
Did you mean: 

Hello again!!! I'm trying to use tne new version of SMT32CubeIDE, it's embarassing to ask if the compiled program can produce the NAME.bin instead of NAME.elf. The STM32-ST-LINK programmer doesn' accept the *.elf. Thanks again for you attention.

INaka.1
Associate III
 
4 REPLIES 4
JTP1
Lead

Hello

Check in the project -> properties output formats you need:


_legacyfs_online_stmicro_images_0693W00000dJylpQAC.png

I thought STM32 Cube Programmer supported .ELF in the writing tab? ST-LINK Utilities is deprecated for MANY YEARS

Add post-build to convert to .BIN (files) or . HEX

.BIN singular can be problematic if image is sparse, describing regions GB apart.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
INaka.1
Associate III

Thank you JTP. Today is Sunday and you're ready to answer.

Best regards, Ilson

Thank you again DeLorean. I'm waiting a answer for tomorrow!!! Aujoud'hui est Dimanche.

Best regards, Ilson