HAL_SPI_Transmit and receive not working properly in STM32f103 bluepill
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-06-30 10:12 AM
Hi,
I am facing issue in communicating the STM32F103 with the ADS131M08 Evaluation board as when i try to read the internal register of the ADS131 after the write operation it show some different value apart from the one i write.
i am also attaching my code in which i have 2 function one is to send command and the other one is ADS131M08_recv_response through which i receive the response and based on that i update my ADS131m08 register so every time after transmit when i try to receive some response it shows some other value.
Attaching is the c file for the code
Pelase help me in solving the bug.
0 REPLIES 0