cancel
Showing results for 
Search instead for 
Did you mean: 

Downloadig Hex or elf file in STM32F103 based BluePill Module

joseph_lengyel_1972
Associate II

Welcome to everyone!
This question concerns the STM32F103CBT6 microcontroller , I have given a "BluePill" module equipped with this microcontroller. When I download the hex or elf file with STM Programer, it downloads nicely, no problem, But! however, it catches itself without any precedent and locks itself, and a message appears that it is only available in Reset mode, the program meter is no longer connected to the microcontroller. Could this be eliminated somehow, so that whenever I want to download something, can I do it without any problems? There should be no microcontroller "locking", etc. . Thank you very much in advance for your help Everyone!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

ST resources are only dedicated to supporting genuine ST products. We are not committed to ensuring that clones/fakes products work properly with the firmware we provide.

We suggest to purchase a genuine products and purchase them from known and trusted distributors.

Thank you for your understanding.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

10 REPLIES 10
Andrew Neil
Super User

Beware that it is highly unlikely that a "Blue Pill" contains a genuine STM32.

 


@joseph_lengyel_1972 wrote:

 it catches itself without any precedent and locks itself, and a message appears that it is only available in Reset mode,


Pardon?

Please post a screenshot of what you actually see.

Also what version of CubeProgrammer, what Operating System, etc

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

 

PS:

And are you using a genuine ST-Link, or a "clone":

https://community.st.com/t5/stm32-mcus/how-to-recognize-a-genuine-st-link-v2-versus-a-cloned-one/tac-p/703663/highlight/true#M965

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

The operating system I use is Windows 10, but it used to do this during Window 7 professional. The STM Programmer I use is the latest version offered by the STM download site. there was an older ST-Link programmer application with it also it shop for prominence ,even after all kinds of updates. I will attach a screenshot of the little text box informing me about this microcontroller "lock". If there is a solution to this ,so that there is no download problem, which I wrote about earlier, eternal gratitude and thanks anyway !

And are you using a genuine ST-Link, or a "clone":

https://community.st.com/t5/stm32-mcus/how-to-recognize-a-genuine-st-link-v2-versus-a-cloned-one/tac-p/703663/highlight/true#M965

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
joseph_lengyel_1972
Associate II

 What I'm using  now a pendrive style STLink-2 Programmer , I think It is a "clone"  . Yes  I know exist original     STLink-2 programmer and this programmer look like white  little box with fine ST logo.  .  


@joseph_lengyel_1972 wrote:

  a pendrive style STLink-2   


As shown in the link I gave, that is definitely a clone - not a genuine ST product.

The ST logo is fake.

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

See also:

https://community.st.com/t5/stm32cubeprogrammer-mcus/stlink-v2-not-recognizing-stm32cubeprogrammer/m-p/618633/highlight/true#M5619

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

If you upload broken code, it will fail.

Start looking at the code. Start debugging the code.

It might help to post in your native language, attach code files and pictures.

Your current description of the problem isn't helping diagnose the real issue.

If all the gear you have is counterfeit it is likely to be difficult experience. Buy a NUCLEO board if your time has value.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

@Tesla DeLorean wrote:

If all the gear you have is counterfeit it is likely to be difficult experience. Buy a NUCLEO board if your time has value.


^^^^ This!! ^^^^

@joseph_lengyel_1972 If you doubt it, see this recent tale of woe resulting from fake gear:

https://community.st.com/t5/stm32-mcus-products/debug-blue-pill-with-stlink-v3minie/m-p/711316#M258517

https://community.st.com/t5/stm32-mcus-products/blue-pill-stm32f1-board-gets-programmed-through-arduino-ide-but/td-p/667923

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Thank you very much for the help with the references! All of them program original STMicroeletronics modules, embedded programmers like the Nucleo family, they like it because otherwise I can't access both at once, so they always use the original ones.