cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_ADC_ConvCpltCallback only called once

nollstead
Associate III

I have a custom board with an STM32WB55CEU6 that I'm programming using the STM32CubeIDE.  I'm struggling with getting the ADC to work in DMA mode.  I can connect via SWD and the while loop runs fine but HAL_ADC_ConvCpltCallback is only triggered once (as confirmed by a breakpoint in that function).

  • Continuous Conversion Mode = Enabled
  • DMA Continuous Requests = Enabled
  • Resolution is 8-bit.  What's connected is a joystick and I just need 0-255
  • DMA set to Circular with data width set to Word

Here is the code.  Nearly all of this was auto-generated by STM32CubeIDE (I removed most of the comment blocks to make it easier to read) - all I really changed was adding in the HAL_ADC_ConvCpltCallback function, a variable to store the results, a call to HAL_ADC_Start_DMA and an LED toggle.  

Any help would be greatly appreciated.  I feel as if I have to be missing something simple but hours into it I can't find it.

 

/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "usb_device.h"


/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;

RTC_HandleTypeDef hrtc;

/* USER CODE BEGIN PV */
uint32_t AD_RES_BUFFER[2];

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
void PeriphCommonClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_ADC1_Init(void);
static void MX_RTC_Init(void);

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc) {

	// Continuous ADC conversion of Analog inputs is complete and stored in the data structure to be used later.
	uint32_t x = AD_RES_BUFFER[0];
	uint32_t y = AD_RES_BUFFER[1];
	uint8_t z = 1;
	x++;
	y++;
	z++;

}

/* USER CODE END 0 */

/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();


  /* Configure the system clock */
  SystemClock_Config();

/* Configure the peripherals common clocks */
  PeriphCommonClock_Config();


  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_DMA_Init();
  MX_USB_Device_Init();
  MX_ADC1_Init();
  MX_RTC_Init();
  /* USER CODE BEGIN 2 */
  HAL_GPIO_WritePin(LED_GPIO_Port, LED_Pin, GPIO_PIN_SET);
  HAL_ADC_Start_DMA(&hadc1, AD_RES_BUFFER, 2);
  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  uint8_t x = 0;
  while (1)
  {
	  x++;
  }
}

/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  /** Configure the main internal regulator output voltage
  */
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSI1
                              |RCC_OSCILLATORTYPE_HSE;
  RCC_OscInitStruct.HSEState = RCC_HSE_ON;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.LSIState = RCC_LSI_ON;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
  RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV2;
  RCC_OscInitStruct.PLL.PLLN = 8;
  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
  RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
  RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure the SYSCLKSource, HCLK, PCLK1 and PCLK2 clocks dividers
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK4|RCC_CLOCKTYPE_HCLK2
                              |RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
  RCC_ClkInitStruct.AHBCLK2Divider = RCC_SYSCLK_DIV2;
  RCC_ClkInitStruct.AHBCLK4Divider = RCC_SYSCLK_DIV1;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
  {
    Error_Handler();
  }
}

/**
  * @brief Peripherals Common Clock Configuration
  * @retval None
  */
void PeriphCommonClock_Config(void)
{
  RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};

  /** Initializes the peripherals clock
  */
  PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SMPS|RCC_PERIPHCLK_USB
                              |RCC_PERIPHCLK_ADC;
  PeriphClkInitStruct.PLLSAI1.PLLN = 6;
  PeriphClkInitStruct.PLLSAI1.PLLP = RCC_PLLP_DIV2;
  PeriphClkInitStruct.PLLSAI1.PLLQ = RCC_PLLQ_DIV2;
  PeriphClkInitStruct.PLLSAI1.PLLR = RCC_PLLR_DIV2;
  PeriphClkInitStruct.PLLSAI1.PLLSAI1ClockOut = RCC_PLLSAI1_USBCLK|RCC_PLLSAI1_ADCCLK;
  PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_PLLSAI1;
  PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_PLLSAI1;
  PeriphClkInitStruct.SmpsClockSelection = RCC_SMPSCLKSOURCE_HSI;
  PeriphClkInitStruct.SmpsDivSelection = RCC_SMPSCLKDIV_RANGE1;

  if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN Smps */

  /* USER CODE END Smps */
}

/**
  * @brief ADC1 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_ADC1_Init(void)
{


  ADC_ChannelConfTypeDef sConfig = {0};

  hadc1.Instance = ADC1;
  hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
  hadc1.Init.Resolution = ADC_RESOLUTION_8B;
  hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
  hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
  hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
  hadc1.Init.LowPowerAutoWait = DISABLE;
  hadc1.Init.ContinuousConvMode = ENABLE;
  hadc1.Init.NbrOfConversion = 2;
  hadc1.Init.DiscontinuousConvMode = DISABLE;
  hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
  hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
  hadc1.Init.DMAContinuousRequests = DISABLE;
  hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
  hadc1.Init.OversamplingMode = DISABLE;
  if (HAL_ADC_Init(&hadc1) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure Regular Channel
  */
  sConfig.Channel = ADC_CHANNEL_15;
  sConfig.Rank = ADC_REGULAR_RANK_1;
  sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
  sConfig.SingleDiff = ADC_SINGLE_ENDED;
  sConfig.OffsetNumber = ADC_OFFSET_NONE;
  sConfig.Offset = 0;
  if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure Regular Channel
  */
  sConfig.Channel = ADC_CHANNEL_16;
  sConfig.Rank = ADC_REGULAR_RANK_2;
  if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }

}

/**
  * @brief RTC Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_RTC_Init(void)
{

  /** Initialize RTC Only
  */
  hrtc.Instance = RTC;
  hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
  hrtc.Init.AsynchPrediv = 127;
  hrtc.Init.SynchPrediv = 255;
  hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
  hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
  hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
  hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
  if (HAL_RTC_Init(&hrtc) != HAL_OK)
  {
    Error_Handler();
  }

  /** Enable the WakeUp
  */
  if (HAL_RTCEx_SetWakeUpTimer(&hrtc, 0, RTC_WAKEUPCLOCK_RTCCLK_DIV16) != HAL_OK)
  {
    Error_Handler();
  }

}

/**
  * Enable DMA controller clock
  */
static void MX_DMA_Init(void)
{

  /* DMA controller clock enable */
  __HAL_RCC_DMAMUX1_CLK_ENABLE();
  __HAL_RCC_DMA1_CLK_ENABLE();

  /* DMA interrupt init */
  /* DMA1_Channel1_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);

}

/**
  * @brief GPIO Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOH_CLK_ENABLE();
  __HAL_RCC_GPIOA_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(LED_GPIO_Port, LED_Pin, GPIO_PIN_RESET);

  /*Configure GPIO pin : Button4_BOOT0_Pin */
  GPIO_InitStruct.Pin = Button4_BOOT0_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  HAL_GPIO_Init(Button4_BOOT0_GPIO_Port, &GPIO_InitStruct);

  /*Configure GPIO pin : LED_Pin */
  GPIO_InitStruct.Pin = LED_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(LED_GPIO_Port, &GPIO_InitStruct);

}


/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}

#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @PAram  file: pointer to the source file name
  * @PAram  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Karl Yamashita
Principal

You've set the ADC to do conversion on software start. You should instead set the ADC conversion to trigger off a timer at an interval. When the conversion is done then HAL_ADC_ConvCpltCallback will be called and then repeat

 

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

View solution in original post

7 REPLIES 7
TDK
Guru

> DMA set to Circular with data width set to Word

For 8 bit ADC values, you should use byte width, not word width.

> sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5

May want to increase that, at least during debugging. You may be stressing the DMA bandwidth available at that rate.

Calling DMA for 2 values is pretty inefficient, especially if it's continuously converting. It will call the half-complete callback on the first value and the full-complete callback on the second. That's 1 callback per conversion. Not going to be able to keep up with callbacks at that rate, especially not with the lowest sampling time.

If you feel a post has answered your question, please click "Accept as Solution".

Thank you for the reply.  My full application will have 7 ADC conversions and send those out via BLE.  Instead of troubleshooting a full app I put together this simple one (with just two analog conversions) to simply things and eliminate other areas of possible conflict.  

I changed to byte - something I was planning anyway, though one of my analog values (voltage monitor) may force me to half-word - and a sampling time of 6.5 but, while probably more efficient (and appreciated) I still have the same problem with the callback only getting fired once.  

Karl Yamashita
Principal

You've set the ADC to do conversion on software start. You should instead set the ADC conversion to trigger off a timer at an interval. When the conversion is done then HAL_ADC_ConvCpltCallback will be called and then repeat

 

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

Ooh I like that Idea. I had planned to look into timers, and wondered if i needed them here) but hadn't gotten there yet - then I could configure a prescaler to control how often it runs, etc.

 

How would I implement the timer part though?  I see "Capture Compare 1 event", Capture Compare 2 event", "Trigger out event", etc.  Any push in the right direction (or resource to read) would be helpful.

 

Forgive the newbie questions as I'm a long-time Arduino developer who is just getting into STM32

OK, I think I figured it out (with the push in the right direction you gave me).  Here is what I did so far:

  • Set external trigger conversion source to "Timer 2 Trigger Out event"
  • Updated settings as follows:
    • TIM Prescaler:  255
    • TIM Counter period:  49999
    • TIM auto-reload preload:  Enable
    • TIM Trigger Event Selection:  Update Event
    • ADC Continuous Conversion Mode:  Disabled
    • DMA Continuous Requests:  Enabled
    • End of Conversion Selection:  End of sequence of conversion 
    • Added a call to HAL_TIM_Base_Start(&htim2) prior to the call to HAL_ADC_Start_DMA

So with that it's now firing every 200ms, which is about what I'm looking for for now.  Very appreciative of the push in the right direction.

If you see anything in the above that seems off feel free to let me know but from what I can tell the problem appears to be solved.

You're welcome. Glad you got it all working. All the settings look like how I'd set them.

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

I got an answer, Thanks a lot!!!