2024-01-21 1:04 PM
Today, I tried installing CubeIDE so I could get a sample project up and running to evaluate against a Nucleo 144 board. This is my second attempt, and both times I get this error. Nothing in the manual, cannot find nothing on Google either.
The IDE is *so* heavy, my mac struggles like notihng I have seen before, closing a window (like the product selector) takes more than 10 seconds where you are locked waiting for it. Not to be deterred I am hoping the experience gets better... although based on past work I will probably end up trying Platform.io which seems far better than the Eclipse based IDEs'
Anyway, frustrations aside, any idea what this error means and how I get past it?
Thanks in advance..
Gerry
Solved! Go to Solution.
2024-01-21 1:10 PM
Hello @gerrysweeney and welcome to the ST Community :smiling_face_with_smiling_eyes:.
This message means that you should login to STM32CUBEIDE to be able to download the software packages that you are going to use on your project.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-21 1:10 PM
Hello @gerrysweeney and welcome to the ST Community :smiling_face_with_smiling_eyes:.
This message means that you should login to STM32CUBEIDE to be able to download the software packages that you are going to use on your project.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-21 1:13 PM
It means you're not logged into the ST support site. Need to log in using the credentials you used to log in here to the forum.
Should be a "MyST" icon in the mid-right tool bar, top of screen. Should bring up browser for you to log in.
2024-01-21 1:30 PM
Ok don't worrk, I eventually found the My ST menu and logged in, that got me past that problem, now I seem to need to find some more tutorials, the ones I found so far show one thing which does not seem to work when I do it.
Sigh.... no wonder arduino had such good takeup..! The barrier to entry with STM32's/ARM is so very high
2024-01-21 1:32 PM
Thank you, I managed to find that, but appreciate the response. I seem to be having a real battle though, solved that problem and immediately run into the next. I don't want to bother the community though with a load of dumb noob questions... would be lovely if the CubeMX/Nucleo boards just worked, but I tell you, its not obvious :(
2024-01-21 1:33 PM
Thank you for your reply, appreciate that. Sorry for the noob question
Gerry
2024-01-21 1:50 PM
Ok so finally after installing the ST-Link Server I managed to program a blinky test program on the green LED of my board and get it programmed and blinking.