cancel
Showing results for 
Search instead for 
Did you mean: 

FreeRTOS and USB givers Hard Fault in H743 MCU

RAbdu.1542
Associate
 

Dear Sirs

I am having a problem using FreeRTOS and USB on H7 series MCU. The IDE gives “Hard Fault” when I debug the project. See image below.

RAbdu1542_1-1708960464673.jpeg

 

The environments are :

STM32CubeIDE:  Version: 1.14.0, Build: 19471_20231121_1200 (UTC)

Target: NUCLEO-H743ZI2

Enclosed herewith are the two “ioc” files.

FreeRTOS_USB1.ioc is for the project without initialization to the USB and it is working fine.

FreeRTOS_USB.ioc is for the project with the initialization to the USB and it is giving my Hard Fault.

 

Your help and assistance are highly appreciated.

Best Regards

Dr Reyah Abdula

 

2 REPLIES 2
FBL
ST Employee

Hi @RAbdu.1542 

Do you still have the same issue if yes, please consider attaching your IOC file.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


Hi FBL

Thank you for the reply. Yes, I am still having the problem. I already attached the IOC files above.

Regards