cancel
Showing results for 
Search instead for 
Did you mean: 

Ethernet not working

QSDFG.1
Associate

Hello community, I'm using

Software:

-STM32CubeIDE v1.10.1-

-STM32Cube FW_F4 V1.27.1

Hardware:

-STM32F4Discovery

-PHY DP83848

-RJ45

I want to implement the Ethernet peripheral in the STM32F407 mcu with RMI mode without RTOS (via polling mode), and I used stm32Cubeide to create the Ethernet project; I just want to ping the board and go from there, but I can't get it to work. I noticed that after many resets of the mcu, the communication can work and I am able to ping. I think that there is a memory issue with the initialization of the LWIP stack. Can anyone give me some solutions to this problem?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0