2023-11-07 3:01 AM
hi everyone, idk if this problem was already reported but i didn't find anything that helped me solving my problem.
i'm using the board B-L475EIOT01A and everytime i try to debug in my STM IDE it tells "no ST Link detected".
can someone pls tell me step-by-step how to solve this problem?
can it be that my pc doesn't see the board?
thanks
2023-11-07 3:06 AM
You'd need to see the board and an ST-LINK in Device Manager. You'd need the right driver, a suitable data cable, and plug into the correct USB port. Check the board provides an ST-LINK, and not an external SWD/JTAG pod.
2023-11-07 3:10 AM
so it's possible that the data cable could be the problem
actually I went to look at Device Manager and it seems that the board is not seen by the PC
also how can i check that the board is providing an ST-LINK
sorry if my questions are trivial but i'm a beginner
2023-11-07 3:10 AM
ST-LINK is on-board via connector in North East top edge. Make sure you have a good cable, not a power-only charger cable.
2023-11-07 3:20 AM
i think everything is working properly, also the cable is the one that my university gave to me.
i read that the problem could be the firmware version, could it be?
idk how to do the update
2023-11-07 3:40 AM
The STM32 Cube Programmer firmware update for the ST-LINK still needs to see the device.
Work with someone who knows how to run Windows.
2023-11-07 3:51 AM
ok thanks