2021-05-16 8:19 AM
Oscilloscope_SignalsGenerator example Not Loading the Kit. i got the Error like
Error in final launch sequence:
Failed to execute MI command:
load E:\\ST\\en.stm32cubeh7_v1-9-0\\STM32Cube_FW_H7_V1.9.0\\Projects\\STM32H735G-DK\\Demonstrations\\Oscilloscope_SignalsGenerator\\STM32CubeIDE\\Debug\\Oscilloscope_SignalsGenerator-STM32H735G-DK_OoB_V1.0.0.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load E:\\ST\\en.stm32cubeh7_v1-9-0\\STM32Cube_FW_H7_V1.9.0\\Projects\\STM32H735G-DK\\Demonstrations\\Oscilloscope_SignalsGenerator\\STM32CubeIDE\\Debug\\Oscilloscope_SignalsGenerator-STM32H735G-DK_OoB_V1.0.0.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load E:\\ST\\en.stm32cubeh7_v1-9-0\\STM32Cube_FW_H7_V1.9.0\\Projects\\STM32H735G-DK\\Demonstrations\\Oscilloscope_SignalsGenerator\\STM32CubeIDE\\Debug\\Oscilloscope_SignalsGenerator-STM32H735G-DK_OoB_V1.0.0.elf
Error message from debugger back end:
Load failed
Load failed
2021-06-04 2:31 AM
Agreed. Multiple ways to do it, which may trigger different background workflows with slightly different results...
2021-06-04 6:26 AM
Double click the Project and this automatically add the workspace
2021-06-04 12:11 PM
Not sure about because according to me your way of working should be ok relying on this kind of example.
Weird stuff is you're getting trouble at debug time not compile time.
Just in case could you get a new try relying on File > Import > General > Import STM32Cube example
Let us know if helping or leading to same trouble.
2021-06-09 7:03 AM
@senthil,
I had some feedback from devs providing the examples that could remove some of the confusion. I copy paste:
-------------
Be carful, the demo was made to have:
- EEMBC® CoreMark® benchmark
Running from internal flash and giving 2777 CoreMark® with CPU at 550MHz
- Oscilloscope/Signals Generator:
- Code Execution from external OctoSPI flash
- LCD display from external OctoSPI RAM
- TouchGFX graphical demonstration
- Code Execution from external OctoSPI flash
- LCD display from external OctoSPI RAM
This Demo MenuLauncher must be programmed into the board first to allow running sub-demonstrations
The menu MenuLauncher will configure the external OctoSPI memories the will allow user to select one of the sub-demo (EEMBC, Oscilloscope or TouchGFX )
So the Oscilloscope linker and VTOR are correct.
Please have look at the readme.txt at the root STM32H735G-DK\Demonstrations folder
-------------
So that could explain issues with linker script, vtor, etc, since the project is supposed to contain a demolauncher!
They however confirmed my suspicion that there is a mix-up of TIM6 and TIM7.
Internal ticket #107323