Debugging fails in CubeIDE
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-13 10:16 PM
Thank you for helping.
environment:
Debugger: ST-LINK V3MINI
STM32CubeIDE Ver1.6.1
STM32CubeProgrammer Ver2.7.0
Board: Custom
I plugged the STM32CubeProgrammer into a custom board and tried connecting 10 times and it succeeded 10 times.
The frequency at this time is 24000kHz.
When I plug in the STM32CubeIDE and try Debug, it only succeeds 3 out of 10 times.
The frequency at this time is 8000kHz.
How can I improve it?
Thank you.
Labels:
- Labels:
-
STM32CubeIDE
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0