cancel
Showing results for 
Search instead for 
Did you mean: 

Debugger connection lost. Shutting down... Not able to find P2PSRV�? device

SSM.2
Associate

STM32 B-U585I-IOT02A

I am getting the below response in IDE when trying to run BLE_AT_CLIENT example in IDE, and not able to get the expected output, i.e Not able to find P2PSRV�? device. as mentioned in the readme file :

 readme: file:///C:/ST/en.stm32cubeu5_v1-1-0/STM32Cube_FW_U5_V1.1.0/Projects/B-U585I-IOT02A/Applications/BLE/BLE_AT_Client/readme.html

File download complete

Time elapsed during download operation: 00:00:01.063

Verifying ...

Download verified successfully 

Debugger connection lost.

Shutting down...

Even the simple demonstration is not working ( file:///C:/ST/en.stm32cubeu5_v1-1-0/STM32Cube_FW_U5_V1.1.0/Projects/B-U585I-IOT02A/Demonstrations/IOT_HTTP_WebServer/readme.html ) The server is not responding.

Please help me out with the solution.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
CMYL
ST Employee

Hello,

Is it the same issue with the simple demonstration ? can you give more details, I will share your issues with colleagues.

Best regards,

Younes