cancel
Showing results for 
Search instead for 
Did you mean: 

Debug configuration for quick DOWNLOAD and RUN

Not applicable

I found this:

Atollic debug configuration for quick DOWNLOAD and RUN

0693W0000000HeGQAU.png

How to set this to STM32CubeIDE?

http://www.emcu.eu/atollic-debug-configuration-for-quick-download-and-run/

2 REPLIES 2
mattias norlander
ST Employee

In CubeIDE 1.3.0 we introduced the "Run button". If you have a working debug configuration. Then you can use the Run button which will take a subset of the parameters from the debug configuration (list of elf-files etc) to only program the device and reset it.

Thanks, it's not the same thing as being able to edit, but it will do.