cancel
Showing results for 
Search instead for 
Did you mean: 

Could not generate the code with STM32cube IDE

nkkaderu
Associate

Could not generate the code while enter Ctrl+S . Getting the error as in the attached image.

3 REPLIES 3
nkkaderu
Associate

Using STM32IDE, Stlink Server

christelle burguera
ST Employee

Hello nkkaderu,

Maybe you project is using a software pack you need to download.

You can check it by opening by doubleclick the ioc file in your project, then check in the Pinout & Configuration view the Middleware and Software Packs you can used for your device.

If you need to download one, you have to be logged. To do it, please click on myST menu.

BR

JackL
Associate

You need to log into your ST account in cubeide ( in my case I used button near help ). After that ide do what it wants (e.g. updates . etc. ) and generates code