cancel
Showing results for 
Search instead for 
Did you mean: 

Compilation Error when Using STM Cube IDE V 1.18

PJose.4
Senior

Hi All
Greetings

Im using the SBSFU folder from b-U585-IOT2A and was successfully running the codes. When updated the cube ide to latest version v1.18 from version v1.17, the following compilation is occuring in the Secure Application
Error message:

"C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v8-m.main+fp/hard\libc_nano.a(libc_a-gettimeofdayr.o): note: the message above does not take linker garbage collection into account"



and the compilation is failing. Anyone could you suggest a fix to this issue

Thanks for the support in advance
Regards
Philip

1 REPLY 1
TDK
Guru

> note: the message above does not take linker garbage collection into account

and what is the message above? Post the full error message.

If you feel a post has answered your question, please click "Accept as Solution".