cancel
Showing results for 
Search instead for 
Did you mean: 

COMP2 not avalialble for H7A3RIT6 on CubeIDE 1.15.1

GMate.11
Associate II

GMate11_0-1716227328695.png

COMP2 is not listed on the configuration tool... eventhough it is well documented on the RM0455.

 

Please provide directions to activate and use properly COMP2 on the H7A3

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @GMate.11 

As you can see on the DS13195, the STM32H7A3RIT6 provide only 1 Comparator (last column of the following screenshot):

Screenshot_2024-05-20-20-24-06-67_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @GMate.11 

As you can see on the DS13195, the STM32H7A3RIT6 provide only 1 Comparator (last column of the following screenshot):

Screenshot_2024-05-20-20-24-06-67_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.