2024-01-31 3:33 AM
Hi
I am using STM32F446ZET6 board but I am unable to generate code. I am facing this issue "Code generation could not be done most probably because the necessary firmware package is missing" I have tried all the process which are mentioned on different platform even on ST community page. I tried to download the firmware package manually and installed it but the error is same. kindly tell me what should I do. STM32CubeIDE version is 1.14.1. and firmware package version is 1.28.0. but nothing is working after every possible solution.
2024-01-31 5:20 AM
Hello @SShah.27
First let me thank you for posting.
In order to overcome this problem please follow those steps:
- First make sure that your STM32CubeIDE is connected to the Internet:
More details could be found in UM2609 section 1.2.3 STM32CubeIDE user authentication.
- Try to uninstall then reinstall STM32CubeIDE .
I will be waiting for your feedback.
Thx
Ghofrane
2024-01-31 6:16 AM
Go into Help -> Manage Embedded Software Packages and install the necessary firmware package.
2024-01-31 9:52 PM
Hi Guru
Thank you for your answer but I have tried this solution as well but in my case its not working.
2024-01-31 9:53 PM
Hello Ghofrane
Thank you for your reply i have connected my stm32cubeide to the internet. also i have uninstalled and installed but its showing same error.
Thnx
2024-01-31 11:59 PM
Hello @SShah.27 ,
I assume you start a project from STM32 Target Selector using Board NUCLEO-F446ZE, right ?
If the code generation tells you the firmware is missing, then the first thing to check is your firmware repository path settings.
Open menu Window > Preferences, then in the window select STM32Cube > Firmware Updater, and check the field Repository Setup. Click Browse to open the selected folder and check its contents for the STM32F4 pack you are using.