Cannot debug with STM32CubeIDE and ST-LINK/V2, but CubeProgrammer works.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-01-12 2:40 PM
I am using STM32CubeIDE version 1.13.2 and an ST-LINK/V2.
I have a custom board with an STM32G031CU86 and I am connecting via SWD.
When I try to either Run or Debug from the IDE, I get an error from the ST-LINK (see below). However, using the STM32CubeProgrammer, I can connect to the ST-LINK, load up the .elf file and program the board just fine.
This makes me think the board and programmer are working correctly, but I'm missing a setting somewhere to make this work. Based on the errors below, it sure smells like a Windows firewall issue, but I can't find anything blocking anything called 'gdb' or 'stlink'. Any ideas?
The Error Message:
Failed to execute MI Command:
target remote localhost:61234
Error message from debugger back end:
localhost:61234: Connection timed out
The following is the console output:
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : C:\Gitclones\usb-c-cable-tester\Firmware\Debug\st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
COM frequency = 4000 kHz
Target connection mode: Attach
Reading ROM table for AP 0 @0xf0000fd0
Hardware watchpoint supported by the target
ST-LINK Firmware version : V2J43S7
Device ID: 0x466
PC: 0xa
ST-LINK device status: RUN_MODE
ST-LINK detects target voltage = 3.21 V
ST-LINK device status: RUN_MODE
ST-LINK device initialization OK
Stm32Device, pollAndNotify running...
SwvSrv state change: 0 -> 1
Waiting for debugger connection...
Waiting for connection on port 61234...
Waiting for connection on port 61235...
Accepted connection on port 61234...
Debugger connected
Waiting for debugger connection...
Waiting for connection on port 61234...
GDB session thread running
GdbSessionManager, session started: 1
Try halt...
GDB session terminated: Client connection lost
GdbSessionManager, session terminated: 1
GdbSrv, last session terminated, signal dispose
Stopping port 61234
Cleanup session: 1
GDB session disposed: 1
ST-LINK device status: HALT_MODE
Received stop for port 61234, not accepting new connections.
GdbSrv, deInit entry.
Shutting down...
GdbSessionManager, deInit entry.
GdbSessionManager, deInit exit
SwvSrv deInit entry
Stopping port 61235
Stopping port 61234
Received stop for port 61235, not accepting new connections.
SwvSrv deInit exit
Stm32Device, closeDevice() entry
Stm32Device, pollAndNotify stopped
Stm32Device, closeDevice() exit
Stm32Device, deInit success
GdbSrv, deInit exit.
Exit.
I'm also attaching my debug configuration in case it helps.
- Labels:
-
STM32CubeIDE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-01-12 2:53 PM
Counterfeit programmers don't work with the newer releases of STM32CubeIDE (but still work with STM32CubeProgrammer). Genuine programmers should work okay.
Does it work with a new project generated from CubeMX?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-01-12 3:02 PM
Is there a way to tell if I have a counterfeit programmer? This thing has the ST logo on the front and an ST-branded label on the back with a serial number and all of the compliance agency marks, etc. Seems like a lot of effort for a $50 programmer (but I guess I've seen worse...)
In case this means anything, the serial number on the label is B 2018 41
Also,
* This project was started with CubeMx (just a blinky light and all of the peripheral configuration functions generated by CubeMx at the moment)
* I disabled all of the Windows Defender firewall settings (Domain Network/Private Network/Public Network) and it still didn't work...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-01-12 3:56 PM
> Is there a way to tell if I have a counterfeit programmer?
There's no perfect test, but if it looks like this one and you bought it from a reputable seller, it's probably real:
https://www.st.com/en/development-tools/st-link-v2.html
As opposed to the "ST-LINK V2" or "ST Link V2" ones on amazon with the 10-pin header which are all counterfeit to some degree.
> I disabled all of the Windows Defender firewall settings (Domain Network/Private Network/Public Network) and it still didn't work...
That would have been my next guess. Could still be the reason if there's a setting you missed somewhere, or some other program at work, but I'm kind of grasping at straws at this point. I'll post again if I think of something else.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-01-12 4:54 PM
Thanks for the help. My programmer looks genuine and came from Mouser, so I'm guessing that is not the problem.
Also, I apparently hit 'solution' with my clumsy trackpad so your previous comment looks like the solution...oops...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-01-12 5:19 PM
I would also guess Mouser sent you a genuine programmer and something else is afoot.
> Also, I apparently hit 'solution' with my clumsy trackpad so your previous comment looks like the solution...oops...
You can flag it if you want (via report inappropriate content) and ask a moderator to remove the "accepted solution". We don't allow users to remove or change it for some reason. Or change it.