cancel
Showing results for 
Search instead for 
Did you mean: 

Can't create a workspace/project with the STM32CubIDE 1.3

WTom
Associate III

Hi,

When I try to create a new workspace in latest STM32CubeIDE 1.3, There is a split second where you see the small disc indicating processing, and then looks like it aborts and nothing happens.

I notice that it can work with existing projects/ workspace created by SW4STM32. So the work around is to create the workspace and copy over the projects with SW4STM32 and continue on STM32CubeIDE as a work around.

Any one else having this problem? Any feedback on this is welcome because with this problem, it's just as productive to stay on SW4STM32.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
WTom
Associate III

I should state this is with MacOS; I also got this message " The application “SetupSTM32CubeMX-5.4.0�? can’t be opened." when trying to open MX from within STM32CubeIDE." The actual MX version used is 5.6.0.

WTom
Associate III

This is with a nucleo G474 board.

Cartu38 OpenDev
Lead III

A bit lost here myself about your comment.

+ You're claiming to rely on STM32CubeIDE but getting some STM32CubeMX installer notification (SetupSTM32CubeMX-5.4.0 is MX tool installer binary name) so ?

+ Sounds you're mixing workspace and project wording. Only way to create an Eclipse workspace is either at application launch or relying on File > Switch Workspace.

Please add some details / snapshots / ... to give community a chance to help you.

WTom
Associate III

Hi Cartu38,

When I talk about the CubeMX program, I'm invoking from the STM32CubeIDE context by clicking on the .ioc file type. In the meantime, I temporarily went back to the SWB environment. Let me see if I can capture more info. when I go back to the STM32CubeIDE environment.

Thanks