2021-07-16 6:32 AM
Here's the scenario:
I have clean workspace. I have two projects on disk I want to import into the workspace. I store them on my Google Drive locally sync'd to my computer (Windows 10).
I import one of the projects and try to build it. I can't because it's looking for dependencies in directories that simply do not exist.
Steps:
File->Import->Existing Projects into Workspace
Select project from file system, and select finish.
Attempt to build project:
make: *** No rule to make target 'C:/ST/STM32CubeIDE_1.6.1/STM32CubeIDE/file/C/Users/username/Google%20Drive/Google Drive/Projects/STM32Cube/Repository/STM32Cube_FW_L4_V1.17.0/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal.c', needed by 'Drivers/STM32L4xx_HAL_Driver/stm32l4xx_hal.o'. Stop.
make: *** Waiting for unfinished jobs....
This project was building fine, but I wanted to rename it.
Now, I can't use it at all. I have multiple projects behaving this way.
I'm not sure what else to do with this, but it's getting me frustrated.
2021-07-16 8:32 AM
It looks like the path in G drive has a form or "file://C/Users/...." etc.
This is of course not valid filename for the compiler.
Must be C:/Users/username.... (can use / or \ )
And no spaces in the path. Spaces in path is begging for trouble.
--pa
2021-07-16 8:48 AM
I have no reference to this path in my project at all.
I was able to fix this project though. I set copy_PARENT to "C:\users\username" in Resource->Linked Resources.
However, that only worked for this project. My other project is complaining:
make: *** No rule to make target 'C:/Users/username/Google Drive/Projects/STM32Cube/Repository/STM32Cube_FW_L4_V1.17.0/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal.c', needed by 'Drivers/STM32L4xx_HAL_Driver/stm32l4xx_hal.o'. Stop.
The only way I've been able to fix this is by making a directory junction in C:/Users/username/Google Drive/Projects/ to C:\Users\username\STM32Cube
I don't understand why it's trying to find the STM32Cube files relative to my Projects folder and not under my username.
2021-07-16 9:53 AM
> The only way I've been able to fix this is by making a directory junction in C:/Users/username/Google Drive/Projects/ to C:\Users\username\STM32Cube
This IMHO is a good solution for Win10. Win10 has also symbolic links.
Things like "copy_PARENT" in .project seem to be caused by glitches in Eclipse importer; these should be fixed and replaced to normal PARENT references.
Maybe edit the .project manually.
It's easier done than explained.
-- pa
2021-07-16 10:07 AM
Thanks. I closed the project in eclipse and changes that variables inside the the .project file. Still works.
I looked at my other project and found that it had a similar discrepancy. Unfortunately, it's still broken.