build STM32L071CBT project with STM32CubeIDE 1.2.1 failed(solve)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-03-28 9:54 PM
Update, choose "gnu11" not c11 for language standard
Hello,
I'm new bird on STM32CubeIDE,
create a new STM32L071CBTX project from STM32CubeIDE
first to configuration our pin definition and another resource than to generation code
and try build the project will get the below error message
but on another STM32F429/CortexM4 project the compiling passed and run well on chip.
I check the IDE with GNU Tools for STM( 7-2018q2 update)
---------------------------------------------------------------------------------------------------------------------
arm-none-eabi-gcc ../Core/Src/sysmem.c -mcpu=cortex-m0plus -std=c11 -g3 -DUSE_HAL_DRIVER -DDEBUG -DSTM32L071xx -c -I../Drivers/CMSIS/Include -I../Core/Inc -I../Drivers/STM32L0xx_HAL_Driver/Inc -I../Drivers/CMSIS/Device/ST/STM32L0xx/Include -I../Drivers/STM32L0xx_HAL_Driver/Inc/Legacy -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage --specs=nano.specs -mfloat-abi=soft -mthumb -o Core/Src/sysmem.o
arm-none-eabi-gcc ../Drivers/STM32L0xx_HAL_Driver/Src/stm32l0xx_hal_tim_ex.c -mcpu=cortex-m0plus -std=c11 -g3 -DUSE_HAL_DRIVER -DDEBUG -DSTM32L071xx -c -I../Drivers/CMSIS/Include -I../Core/Inc -I../Drivers/STM32L0xx_HAL_Driver/Inc -I../Drivers/CMSIS/Device/ST/STM32L0xx/Include -I../Drivers/STM32L0xx_HAL_Driver/Inc/Legacy -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage --specs=nano.specs -mfloat-abi=soft -mthumb -o Drivers/STM32L0xx_HAL_Driver/Src/stm32l0xx_hal_tim_ex.o
../Core/Src/syscalls.c:66:27: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'asm'
register char * stack_ptr asm("sp");
^~~
Info: Parallel threads used: 8
12:45:27 Build Failed. 1 errors, 0 warnings. (took 4s.78ms)
../Core/Src/sysmem.c:55:27: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'asm'
register char * stack_ptr asm("sp");
^~~
../Core/Src/sysmem.c: In function '_sbrk':
../Core/Src/sysmem.c:65:18: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'asm'
extern char end asm("end");
^~~
../Core/Src/sysmem.c:65:18: warning: implicit declaration of function 'asm' [-Wimplicit-function-declaration]
../Core/Src/sysmem.c:70:15: error: 'end' undeclared (first use in this function)
heap_end = &end;
^~~
../Core/Src/sysmem.c:70:15: note: each undeclared identifier is reported only once for each function it appears in
../Core/Src/sysmem.c:73:24: error: 'stack_ptr' undeclared (first use in this function)
if (heap_end + incr > stack_ptr)
Solved! Go to Solution.
- Labels:
-
STM32CubeIDE
-
STM32L0 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-03 4:51 AM
@Amel NASRI , okay, update best answer,
must to pick up 'GNU11' in language standard options to enable GNU extensions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-01 8:39 AM
Hi @kunyi ,
Glad that you resolved your problem.
But it should be better to add the solution in a separate comment and select it as a best answer.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-03 4:51 AM
@Amel NASRI , okay, update best answer,
must to pick up 'GNU11' in language standard options to enable GNU extensions