cancel
Showing results for 
Search instead for 
Did you mean: 

Bug in X-Cube-AZRTOS-H7 V3.3.0

Intector
Associate III

Hello STM-Team,

I'm working on my project with an STM32H723ZG and ran into an issue with the code generation when I selected "Network Interfaces" in the  AZRTOS configuration.

Intector_1-1733095953265.png

The code generation will add "NX_ETH_INTERFACE_ENABLED" to the "RTE_Components.h" but forget the "#define" in front of it.

Intector_2-1733096278529.png

 

That is somewhat annoying because I have to manually add this everytime I regenerate the code.

 

 

 

0 REPLIES 0