2023-05-25 4:26 AM
Dear,
Microcontroler STM32H742 (stm32CubeIDE)
When i plug out and plug in device, this printing on UART_3:
ţ˙ţţţţţţţţüţüüüüüüüüüüüüüüüüüü
or:
ţ
NVT: FF FE FE
ţţ{FF}
i this problem was not watched on same device with stm32F205(Rowley crossworks).
I clear all buffer
char bufRcv[256] {'\0'}; but it nothing change
Could you have some solution
Many thanks
2023-05-25 7:32 AM
> I mean Plug the power cord to the mains.
> I have RS232 on mainboard in computer and i use db9 cable.
> problem is only after Plug the power cord to the mains.
Don't transmit anything in the STM32 software, just unplug and plug. Still receiving strange characters? Then you a hardware-related problem: observe the line using oscilloscope during unplugging/plugging in. What exactly happens during power-up depends on how exactly the power source and the interface circuitry is designed.
JW
2023-05-26 3:21 AM
Okay, we're getting closer...
Still missing:
2023-06-06 12:17 AM
Sorry for the delay, I was sick.
//--------------------------------------------------------------------------------------
void UART_3::Init()
{
__HAL_RCC_DMA1_CLK_ENABLE();
HAL_NVIC_SetPriority(DMA1_Stream3_IRQn, 3, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream3_IRQn);
/* Peripheral interrupt init */
HAL_NVIC_SetPriority(USART3_IRQn, 2, 0);
HAL_NVIC_EnableIRQ(USART3_IRQn);
__HAL_UART_ENABLE_IT(&huart3,UART_IT_RXNE);
}
//--------------------------------------------------------------------------------------
void UART_3::ParametersChanged()
{
ConfigureUsart();
}
//--------------------------------------------------------------------------------------
void UART_3::ConfigureUsart()
{
uint16_t parity = DecodeParity(Params.Com1_Parity);
huart3.Instance = USART3;
huart3.Init.BaudRate = DecodeBaudrate(Params.Com1_Baudrate);
huart3.Init.WordLength = (parity == PARITY_NONE) ? UART_WORDLENGTH_8B : UART_WORDLENGTH_9B;
huart3.Init.StopBits = UART_STOPBITS_1;
huart3.Init.Parity = parity;
huart3.Init.Mode = UART_MODE_TX_RX;
huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart3.Init.OverSampling = UART_OVERSAMPLING_16;
huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart3.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart3) != HAL_OK) Error_Handler();
if (HAL_UARTEx_SetTxFifoThreshold(&huart3, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK) Error_Handler();
if (HAL_UARTEx_SetRxFifoThreshold(&huart3, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK) Error_Handler();
if (HAL_UARTEx_DisableFifoMode(&huart3) != HAL_OK) Error_Handler();
}
//--------------------------------------------------------------------------------------
2023-06-06 1:03 AM
//--------------------------------------------------------------------------------------
extern "C" void USART3_IRQHandler(void)
{
	if (__HAL_UART_GET_FLAG(&huart3, UART_FLAG_ORE))
	{
		__HAL_UART_CLEAR_FLAG(&huart3, UART_CLEAR_OREF);
	}
 if(__HAL_UART_GET_IT_SOURCE(&huart3,UART_IT_RXNE) != RESET && __HAL_UART_GET_FLAG(&huart3, UART_FLAG_RXNE) != RESET )
 {
		 char data = huart3.Instance->RDR & (uint8_t)0x00FF;
		 Com1.ByteReceivedIsr(data);
}
	HAL_DMA_IRQHandler(&hdma_usart3_tx);
}
 2023-06-06 1:15 AM
__attribute__((weak)) int _write(int file, char *ptr, int len)
{
int DataIdx;
for (DataIdx = 0; DataIdx < len; DataIdx++)
{
__io_putchar(*ptr++);
}
return len;
}
2023-06-06 4:11 AM
There is still no link to the UART whatsoever.
So the _write function needs some output to the UART, like you give the pointer and length to the UART DMA transmit function.
2023-06-06 4:16 AM
Uart still work, this problem is only when plug the power cord to the mains, after start all transmition work correctly.
2023-06-06 4:45 AM
Try to disable bootloader. This is the first FW which can use UART.
2023-06-06 5:52 AM
You're right, i forget