cancel
Showing results for 
Search instead for 
Did you mean: 

ADC on H7 series

anonymous_stm
Associate II

HI,

I am trying to get ADC read but the result is only the first read repeatedly even I change the voltage on ADC channel input it remains the same, 

ADC Innitialization

static void MX_ADC3_Init(void)

{

 

/* USER CODE BEGIN ADC3_Init 0 */

 

/* USER CODE END ADC3_Init 0 */

 

ADC_ChannelConfTypeDef sConfig = {0};

 

/* USER CODE BEGIN ADC3_Init 1 */

 

/* USER CODE END ADC3_Init 1 */

 

/** Common config

*/

hadc3.Instance = ADC3;

hadc3.Init.Resolution = ADC_RESOLUTION_16B;

hadc3.Init.ScanConvMode = ADC_SCAN_DISABLE;

hadc3.Init.EOCSelection = ADC_EOC_SINGLE_CONV;

hadc3.Init.LowPowerAutoWait = DISABLE;

hadc3.Init.ContinuousConvMode = ENABLE;

hadc3.Init.NbrOfConversion = 1;

hadc3.Init.DiscontinuousConvMode = DISABLE;

hadc3.Init.ExternalTrigConv = ADC_SOFTWARE_START;

hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;

hadc3.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;

hadc3.Init.Overrun = ADC_OVR_DATA_PRESERVED;

hadc3.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;

hadc3.Init.OversamplingMode = DISABLE;

if (HAL_ADC_Init(&hadc3) != HAL_OK)

{

Error_Handler();

}

 

/** Configure Regular Channel

*/

sConfig.Channel = ADC_CHANNEL_9;

sConfig.Rank = ADC_REGULAR_RANK_1;

sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;

sConfig.SingleDiff = ADC_SINGLE_ENDED;

sConfig.OffsetNumber = ADC_OFFSET_NONE;

sConfig.Offset = 0;

sConfig.OffsetSignedSaturation = DISABLE;

if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)

{

Error_Handler();

}

/* USER CODE BEGIN ADC3_Init 2 */

 

/* USER CODE END ADC3_Init 2 */

 

}

 

Main Loop

 

while(1)

{

 

HAL_ADC_Start(&hadc3);

 

uint16_t currentADCValue=HAL_ADC_GetValue(&hadc3);

 

 

 

sprintf(disp,"D1: %d\n\r",currentADCValue);

HAL_UART_Transmit(&huart8, (uint8_t*)disp, sizeof(disp), HAL_MAX_DELAY);

}

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User
  • Disable data cache, or manage it properly.
  • ADC data should be a uint16_t.
  • Wait for the ADC to be complete before sending out data. A small delay would be sufficient.

See a working example using HAL_ADC_DMA_Start here:

https://github.com/STMicroelectronics/STM32CubeH7/blob/96dd7e5b69d2b10406ac3f358e44b14cececa611/Projects/NUCLEO-H743ZI/Examples/ADC/ADC_DMA_Transfer/Src/main.c

 

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

4 REPLIES 4
harry123
Senior II

while(1)

{

 

HAL_ADC_Start(&hadc3);

HAL_ADC_PollForConversion(&hadc3,HAL_MAX_DELAY);

uint16_t currentADCValue=HAL_ADC_GetValue(&hadc3);

 

 

 

sprintf(disp,"D1: %d\n\r",currentADCValue);

HAL_UART_Transmit(&huart8, (uint8_t*)disp, sizeof(disp), HAL_MAX_DELAY);

}

anonymous_stm
Associate II

That worked for me, with continuous mode disabled, but when I try to read two and continuous mode enabled and scan conversion mode enabled and with DMA to circular and full word setting I get only zeros. 

the ranking for channels and regular conversions is enabled.

while(1)

{

uint32_t currentADCValue[2]={0};

HAL_ADC_DMA_Start(&hadc3,currentADCValue,2);

sprintf(disp,"D1: %ld D2: %ld\n\r",currentADCValue[0],currentADCValue[1]);

HAL_UART_Transmit(&huart8, (uint8_t*)disp, sizeof(disp), HAL_MAX_DELAY);

}

 

TDK
Super User
  • Disable data cache, or manage it properly.
  • ADC data should be a uint16_t.
  • Wait for the ADC to be complete before sending out data. A small delay would be sufficient.

See a working example using HAL_ADC_DMA_Start here:

https://github.com/STMicroelectronics/STM32CubeH7/blob/96dd7e5b69d2b10406ac3f358e44b14cececa611/Projects/NUCLEO-H743ZI/Examples/ADC/ADC_DMA_Transfer/Src/main.c

 

If you feel a post has answered your question, please click "Accept as Solution".
FBL
ST Employee

Hello @anonymous_stm 

It should be HAL_ADC_Start_DMA instead of HAL_ADC_DMA_Start

To use correctly HAL_ADC_DMA_Start() function, you need to check its definition. 

HAL_StatusTypeDef HAL_ADC_Start_DMA(ADC_HandleTypeDef *hadc, uint32_t *pData, uint32_t Length)

* @param pData Destination Buffer address.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL