2023-12-02 11:50 PM - edited 2023-12-02 11:59 PM
After i generating code from cube MX
This symptom is after updating the IDE to version 1.14.0 and Cube MX version 6.8.1.
In circle from the picture I attached. Can it be fixed or Can it be reset?
Can compile normally But it disturbs the eyes.
Thank you in advance.
TAK
Solved! Go to Solution.
2023-12-03 12:07 AM
Probably a "Display White Space" type setting in the configuration of the editor or screen view options.
2023-12-03 12:07 AM
Probably a "Display White Space" type setting in the configuration of the editor or screen view options.
2023-12-03 12:40 AM
It works now, thank you very much for the advice. :thumbs_up: