cancel
Showing results for 
Search instead for 
Did you mean: 

A big problem with Live Expression (values shifted down)

Alaa_Alnasef96
Associate

I have a problem with CubeIde (version independent tried on both 1.13 and 1.16)

the problem is that in live expression I am using a struct to combine each task in single struct for debugging purpose
the values of the variables all shifted down 
example:
var1: 0
var2: value of var1
var3: value of var2
char arr[100]: [value of var3
                        value of arr[0]
etc]

I am using threadx, the problem doesnot exist when working on UBUNTU while in windows is happening all time.
the other thread values are correct, it happen only on the second thread.

 

/* Includes ------------------------------------------------------------------*/
#include "app_threadx.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "main.h"
#ifdef ExampleProtocole
#include "ExampleCommunicationTask.h"
#endif
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#ifndef URMETPROTOCOL
#define MAIN_THREAD_STACK_SIZE					4096
#elif defined(URMETPROTOCOL)
#define MAIN_THREAD_STACK_SIZE					4096
#define Example_COMMUNICATION_THREAD_STACK_SIZE	4096
#endif
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
uint8_t main_thread_stack[MAIN_THREAD_STACK_SIZE];
TX_THREAD mainThreadPointer;
#if defined(ExamplePROTOCOL)
uint8_t urmet_thread_stack[Example_COMMUNICATION_THREAD_STACK_SIZE];
TX_THREAD exampleCommunicationPointer;
#endif
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
/* USER CODE BEGIN PFP */
static void MainThreadEntry(uint32_t initialInput);
#if defined(ExamplePROTOCOL)
static void ExampleCommunicationThreadEntry(uint32_t initialInput);
#endif
/* USER CODE END PFP */

/**
 * @brief  Application ThreadX Initialization.
 * @PAram memory_ptr: memory pointer
 * @retval int
 */
UINT App_ThreadX_Init(VOID *memory_ptr) {
	UINT ret = TX_SUCCESS;
	/* USER CODE BEGIN App_ThreadX_MEM_POOL */

#ifdef ExamplePROTOCOL

#endif
	/* USER CODE END App_ThreadX_MEM_POOL */
	/* USER CODE BEGIN App_ThreadX_Init */
	if (tx_thread_create(&mainThreadPointer, (char*)"MainThread",
			MainThreadEntry, 0x1234, main_thread_stack,
			MAIN_THREAD_STACK_SIZE, 15, 15, 1,
			TX_AUTO_START) != TX_SUCCESS) {
		return TX_THREAD_ERROR;
	}
#ifdef ExamplePROTOCOL
	if (tx_thread_create(&exampleCommunicationPointer, (char*)"ExampleCommunicationThread",
			exampleCommunicationThreadEntry, 0x1234, example_thread_stack,
			Example_COMMUNICATION_THREAD_STACK_SIZE, 15, 15, 1,
			TX_AUTO_START) != TX_SUCCESS) {
		return TX_THREAD_ERROR;
	}
#endif
	/* USER CODE END App_ThreadX_Init */

	return ret;
}

/**
 * @brief  MX_ThreadX_Init
 * @PAram  None
 * @retval None
 */
void MX_ThreadX_Init(void) {
	/* USER CODE BEGIN  Before_Kernel_Start */

	/* USER CODE END  Before_Kernel_Start */

	tx_kernel_enter();

	/* USER CODE BEGIN  Kernel_Start_Error */

	/* USER CODE END  Kernel_Start_Error */
}

/* USER CODE BEGIN 1 */
void MainThreadEntry(uint32_t initialInput) {
	MainThreadFunction();
}
#ifdef ExamplePROTOCOL
void ExampleCommunicationThreadEntry(uint32_t initialInput) {
	ExampleThread();
}

 


screenshot of the problem 

 

Alaa_Alnasef96_1-1722428599371.png

where as you can see firstrun should be 1 and firstZDAGps is also 1 so we have everthing is shifted down. 

2 REPLIES 2
Mahmoud Ben Romdhane
ST Employee

Hello @Alaa_Alnasef96 ,

 

Welcome to the ST Community and let me thank you for reporting this issue.

I am escalating an internal ticket to the concerned team (ticket number: 201886)

 

Best Regards.

Mahmoud

 

 

Hello @Alaa_Alnasef96 ,

Further to your comment, I recommend that you set the variable format on Live Expression by clicking on Number Format.

MahmoudBenRomdhane_0-1740040899232.png

Thanks.

Mahmoud