2025-01-29 08:55 PM - last edited on 2025-01-30 12:56 AM by Andrew Neil
Edit By ST Moderator: Title of this post has been translated from Chinese to comply with the ST Community guidelines.
2025-01-29 11:30 PM - edited 2025-01-29 11:31 PM
Welcome @xjmxjc, to the community!
The problem is most likely due to the non-ASCII characters you are using in the path.
To test and confirm this, you do not need to reinstall the firmware, but can:
Hope that helps?
Good luck!
/Peter
2025-01-30 12:01 AM
2025-01-30 01:57 AM
In which path did you install the IDE?
2025-01-30 02:06 AM
I first downloaded the IDE from the official website(st.com) on January 16th, and was able to use it normally for study and writing purposes within the following week.
E:ST/STM32CubeIDE_1.17.0
2025-01-30 02:52 AM
So you were able to work with it after the installation?
With which MCU was that and with which firmware library?
You can also download the firmware library a second time, unpack it manually into a different directory (slightly different directory name) and make a binary directory comparison with a suitable tool. Alternatively, change the path to that new directory as a test and try again with the CubeIDE.