cancel
Showing results for 
Search instead for 
Did you mean: 

vscode STM32H7 dualcore project

Jack Mitchel
Associate

How to set up a project for a nucleoH745 so in vscode, with the official stm32 extension, the project can be opened and both subproject are visible and manageable?

Preparation: vscode, extension, STMCUFinder, STM32CubeMX, Git are installed.

How to configure the project in STM32CubeMX so it can be used in vscode?

I managed to create a project, getting one directory with two sub directories in each is a project file.

However, in eclipse the project would be represented as one project with two subprojects. How to achieve this in vscode with the official extension?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0