cancel
Showing results for 
Search instead for 
Did you mean: 

Would like to be able to use Build Analyzer.

Hollies
Associate II

I hope to use the same Build Analyzer in VSCode as in the IDE, which allows developers to more clearly see the use of flash and memory. I have tried to use GPT to write a plugin, but the effect is not good, and I don't understand the JS language well, so it is difficult to develop it by myself.

My mother tongue is not English, please forgive me if it is not easy to understand.

Hollies_0-1721909647932.png

 

14 REPLIES 14

Looks very nice!

Is this an add-in to VS Code?

Just a small suggestion: memory sub areas could perhaps be indended under the parent area?

 

 

Yes, here is a link to the VSCode Marketplace

Feel free to write whatever you think about it. I have no idea how to make plugins, it all happened by accident. I was just very disappointed when I started taking my first steps in VSCode for STM32 and didn't find such a useful tool. The layout is far from perfect, but at least it responds to clicks, expands and collapses)) It's a big success for me. Indents are important, 100% agree

2.JPG

 

quick patch, v.1.0.2 

Great, the devil is in the details! 

You've developed a really useful plugin. I admire your executive ability. Unlike me, I left my work halfway.