Skip to main content
bibble235
Associate III
June 24, 2023
Question

Memory View VS Code

  • June 24, 2023
  • 2 replies
  • 5972 views

Hi,

With VS Code I want to use the memory view which works fine for decimal. 

bibble235_0-1687569406473.png

But does not seem to work if I have 0x20000000.

Here is my launch.json in case

 

 {
 "name": "Launch2",
 "type": "cppdbg",
 "request": "launch",
 "cwd": "${workspaceFolder}",
 "program": "${command:cmake.launchTargetPath}",
 "MIMode": "gdb",
 "miDebuggerPath": "${command:vscode-embedded.st.gdb}",
 "miDebuggerServerAddress": "localhost:3333",
 //"debugServerPath": "${command:vscode-embedded.st.gdbserver}",
 "debugServerPath": "/opt/st/stm32cubeclt_1.12.1/STLink-gdb-server/bin/ST-LINK_gdbserver",
 
 "debugServerArgs": "--stm32cubeprogrammer-path ${command:vscode-embedded.st.cubeprogrammer} --swd --port-number 3333",
 "serverStarted": "Waiting for connection on port .*\\.\\.\\.",
 "stopAtConnect": true,
 "postRemoteConnectCommands": [
 {
 "text": "load ./build/debug/build/Test7.elf"
 }
 ],
 "logging": {
 "engineLogging": true
 },
 "preLaunchTask": "Build",
 "svdPath": "/opt/st/stm32cubeclt_1.12.1/STMicroelectronics_CMSIS_SVD/STM32F302.svd",
 },

 

Thanks

This topic has been closed for replies.

2 replies

KnarfB
Super User
June 24, 2023

Works for me if I enter 0x20000000 after pressing the + (Add new memory view).

Default stm32-for-vscode generated launch file used:

 

{
 "configurations": [
 {
 "showDevDebugOutput": "parsed",
 "cwd": "${workspaceRoot}",
 "executable": "./build/NUCLEO-L432KC.elf",
 "name": "Debug STM32",
 "request": "launch",
 "type": "cortex-debug",
 "servertype": "openocd",
 "preLaunchTask": "Build STM",
 "device": "stm32l432",
 "configFiles": [
 "openocd.cfg"
 ],
 "svdFile": "STM32L4x2.svd"
 }
 ]
}

 

I can even enter &_sdata and see the RAM (depending on your .ld file).

Check your Debug Console tab for suspicious output.

hth

KnarfB

bibble235
bibble235Author
Associate III
June 24, 2023

It is strange and probably cortex-debug than stm32. On linux so may try them. Think I can manage with converting to decimal online