2024-03-20 2:23 AM
Shed some light on STM32WL5MOC module, when was it introduced, can we implement DASH7 protocol on it?
2024-03-20 2:43 AM
ST32WL5M was released January this year. we don't see a problem in using the Dash7 protocol with WL. The downside is that it is not officially supported by us, so the implementation/porting is up to the customer. From technical point of view we don't see a blocking point. Dash7 uses GFSK modulation, which is supported by the WL, so it is matter of software implementation.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.