2025-05-26 4:00 AM - last edited on 2025-05-26 9:55 AM by Amel NASRI
Hi,
Dual FOC not introduced on STM32F7 series is it due to being not implemented or peripheral of the STM32F7 series(limitations) does not supported?
Thanks,
Rahul D
2025-06-02 3:09 AM
One more question, as stm32f4 series does not supports cordic processor then in motor control workbench 6.4.0 how it shows the option for sensorless speed measurement using cordic processor. When i select sensorless using PLL motor rotates properly but with cordic gives jerks? I am using stm32f4 series controller.