cancel
Showing results for 
Search instead for 
Did you mean: 

Is STMH7 primarily designed to be used with external Flash/Ram only?

Amelie ACKERMANN
Community manager

With the new STMH7 chips, are they primarily designed to be used with external Flash/Ram only? Or is there more onboard than just the 64k Boot Flash?

1 REPLY 1
Roman LUDIN
ST Employee

Hello, On H7R/S is only 64kB Flash for user. This device was intended to be used with external flash or if the application fit into 64kB. For need of internal flash we have classical H7 lines.