cancel
Showing results for 
Search instead for 
Did you mean: 

Can I use the TouchGFX IDE and the new NeoChromVG for any display?

Amelie ACKERMANN
Community manager

Can I use the TouchGFX IDE and the new NeoChromVG for any display? Or are they limited to the displays that are currently embedded Nucleo boards? Is this easy to implement for general displays?

1 REPLY 1
Roman LUDIN
ST Employee

Yes TouchGFX supports NeoChrome VG. Vector graphics is support from TouchGFX V 4.23. This solution could be used with any display. The Microcontrollers STM32U5F9/G9 has the New Chrome VG. We have a couple of boards as reference using STM32U5F9/G9: STM32U5G9J-DK1 and STM32U5G9J-DK2. STM32U5F9/G9 have MIPI-DSI and RGB interfaces besides can support other simpler as SPI or parallel .