2019-05-15 07:22 AM
When trying to flash OpenSTLinux on the STM32MP157C-DK2 the flashing procedure gets halted with the following error message.
16:01:00 : STM32CubeProgrammer API v2.1.0
16:01:01 : USB speed : High Speed (480MBit/s)
16:01:01 : Manuf. ID : STMicroelectronics
16:01:01 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
16:01:01 : SN : 000000000000
16:01:01 : FW version : 0x011a
16:01:01 : Device ID : 0x0500
16:01:19 : Read TSV File: C:\Users\Ludwig\Downloads\en.FLASH-stm32mp1-openstlinux-4.19-thud-mp1-19-02-20\stm32mp1-openstlinux-4.19-thud-mp1-19-02-20\images\stm32mp1\flashlayout_st-image-weston\FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv
16:01:19 : Number of partitions: 9
16:01:40 : Start Embedded Flashing service
16:01:40 : Memory Programming ...
16:01:40 : Opening and parsing file: tf-a-stm32mp157c-dk2-trusted.stm32
16:01:40 : File : tf-a-stm32mp157c-dk2-trusted.stm32
16:01:40 : Size : 245360 Bytes
16:01:40 : Partition ID : 0x01
16:01:40 : Download in Progress:
16:01:40 : File download complete
16:01:40 : Time elapsed during download operation: 00:00:00.630
16:01:40 : RUNNING Program ...
16:01:40 : PartID: :0x01
16:01:41 : Start operation done successfully at partition 0x01
16:01:41 : Flashlayout Programming ...
16:01:41 : Running Flashlayout Partition ...
16:01:41 : Flashlayout partition started successfully
16:01:41 : Memory Programming ...
16:01:41 : Opening and parsing file: u-boot-stm32mp157c-dk2-trusted.stm32
16:01:41 : File : u-boot-stm32mp157c-dk2-trusted.stm32
16:01:41 : Size : 748660 Bytes
16:01:41 : Partition ID : 0x03
16:01:41 : Download in Progress:
16:01:42 : File download complete
16:01:42 : Time elapsed during download operation: 00:00:01.138
16:01:42 : RUNNING Program ...
16:01:42 : PartID: :0x03
16:01:42 : reconnecting the device ...
16:02:12 : Error: unable to reconnect the target device: time out expired
16:02:12 : Error: Start operation failed at partition 0x03
16:02:12 : Error: TSV flashing service failed
16:02:12 : Warning: Connection to device 0x500 is lost
While researching, I stumbled over this particular thread: https://community.st.com/s/question/0D50X0000AgE1buSQC/cant-flash-sd-card-on-stm32mp157xev1-process-stops . This guy had a similar problem as I do. My MB1272 is also green instead of blue like on all the images I saw. This device was provided to me as a part of an urgent project, but I can't seem to get it working. Please provide a solution for me, so I can start working. Thanks to anyone in advance!
2019-05-28 01:54 AM
Sent a Private Message to you. Note that most Alpha HW are not supported by official delivery.
2019-11-13 12:08 PM
I have the same issue as above with STM32MP157C-DK2.
My log is below:
12:03:28 : STM32CubeProgrammer API v2.2.0
12:03:35 : USB speed : High Speed (480MBit/s)
12:03:35 : Manuf. ID : STMicroelectronics
12:03:35 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
12:03:35 : SN : 0046003E3338510634383330
12:03:35 : FW version : 0x0110
12:03:35 : Device ID : 0x0500
12:03:41 : Read TSV File: D:\Projects\Tag\stm32MP1\stm32mp1-openstlinux\images\stm32mp1\flashlayout_st-image-weston\FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv
12:03:41 : Number of partitions: 9
12:03:59 : Start Embedded Flashing service
12:03:59 : Memory Programming ...
12:03:59 : Opening and parsing file: tf-a-stm32mp157c-dk2-trusted.stm32
12:03:59 : File : tf-a-stm32mp157c-dk2-trusted.stm32
12:03:59 : Size : 245364 Bytes
12:03:59 : Partition ID : 0x01
12:03:59 : Download in Progress:
12:04:00 : File download complete
12:04:00 : Time elapsed during download operation: 00:00:00.534
12:04:00 : RUNNING Program ...
12:04:00 : PartID: :0x01
12:04:00 : Start operation done successfully at partition 0x01
12:04:00 : Flashlayout Programming ...
12:04:00 : Running Flashlayout Partition ...
12:04:00 : Flashlayout partition started successfully
12:04:00 : Memory Programming ...
12:04:00 : Opening and parsing file: u-boot-stm32mp157c-dk2-trusted.stm32
12:04:00 : File : u-boot-stm32mp157c-dk2-trusted.stm32
12:04:00 : Size : 805514 Bytes
12:04:00 : Partition ID : 0x03
12:04:00 : Download in Progress:
12:04:01 : File download complete
12:04:01 : Time elapsed during download operation: 00:00:00.992
12:04:01 : RUNNING Program ...
12:04:01 : PartID: :0x03
12:04:01 : reconnecting the device ...
12:04:31 : Error: unable to reconnect the target device: time out expired
12:04:31 : Error: Start operation failed at partition 0x03
12:04:31 : Error: TSV flashing service failed
12:04:31 : Warning: Connection to device 0x500 is lost
12:04:32 : Disconnected from device.
2019-11-13 11:53 PM
please provide a log of the console output (VCP over ST-Link USB micro-B connector)
2019-11-14 03:35 PM
When I installed driver for VCP I was able to flash Linux image and it is working now.
But I have other issue.
I would like to flash and debug Cortex M4 but STMCubeProgrammer says "No stlink detected".
I have tried to install drivers "en.stsw-link009" but still the same.
but I see "ST-Link Debug" on Device Manager.
Thanks.
2019-11-14 11:29 PM
Code upload and development on Cortex-M4 is not done using STM32CubeProgrammer. You should use an IDE such as STM32CubeIDE or SW4STM32.
You have choice to debug Cortex-M4 with Linux up and running from Flash (called 'production mode') or in standalone (called 'Engineering mode')
and https://wiki.st.com/stm32mpu/wiki/STM32-CoPro-MPU_plugin_for_SW4STM32 (SystemWorkbench is going to be deprecated, but you have details about Engineering mode use case)
See also https://wiki.st.com/stm32mpu/wiki/STM32CubeMP1_development_guidelines
2019-11-15 05:16 PM
Thanks for answer.
I was able to debug M4 via VisualGDB but now I got other question.
Is it any way I can start M4 core and run firmware when power applied without starting A7 cores?
I saw that manual says that A7 should reset M4 and load it's binary to the memory first but
I like to double check.
We want to migrate from stm32 Cortex M3 mcu to MP1 but running Linux should be optional in our case
only when we need to do some heavy computations.
2019-11-18 05:32 AM
At cold boot, only A7 will start. As described, it is responsible to load M4 FW and start it. Then A7 could go in low power modes if no Linux required.
At low power exit (e.g. STANDBY), M4 could start from RETRAM code without any A7 action (which can then be woken up later by M4 FW when Linux procession is required).
In short, M4 cannot start from flash as MCUs.
2019-11-18 11:56 AM
Thank you for help.
When A7 is in low power mode can DDR RAM be powered off completely but M4 still running?
Also I understand that A7 could load and reset M4 in UBoot and go low power mode even without linux kernel started
and M4 can wake A7 up after to boot linux. Is it right?
Other question is when M4 reboots (watchdog or so) is it possible to keep firmware in memory? Otherwise if A7 is in deep sleep we will just stuck there.
Thanks.
2019-11-19 12:16 AM
When A7 is in CSTANDBY mode, it is possible to shutdown the DDR instead of keeping it in SR. This is not the defaut OpenSTLinux behavior. https://wiki.st.com/stm32mpu/wiki/Power_overview
At cold power on, A7 could load and start M4 in uBoot (this is an option, default is Linux), but Linux will start anyway, and could go in low power later on. see https://wiki.st.com/stm32mpu/wiki/Boot_chains_overview#Coprocessor_firmware
On platform STANDBY mode wake-up, A7 could stay in CSTANDBY (in fact, it is shortly powered-up and go immediately in low power) while M4 could be started from RETRAM (as other SRAM content are lost in STANDBY). Otherwise, xx-Stop mode should be used to keep VDDCORE, and so, SRAM contents.
M4 cannot reboot itself on a watchdog, remind that M4 is seen as a Linux coprocessor. M4 watchdog is signaled to A7 (with wake up if required), then A7 could restart the M4 or restart the whole platform (this is your implementation choice). global watchdog could also be used to restart the platform.
see https://wiki.st.com/stm32mpu/wiki/How_to_retrieve_Cortex-M4_logs_after_crash