We are pleased to announce to you that the release 6.13.0 of STM32CubeMX is available.
What is new in 6.13.0:
- Added support for the following series, microcontrollers and microprocessors:
STM32U3, STM32WL3x, STM32G411xx and STM32C0
- Added the support for the following Nucleo boards: NUCLEO-C051C8, NUCLEO-C092RC, NUCLEO-U385RG-Q, NUCLEO-WL33CC1 and NUCLEO-WL33CC2
- Added the support for a new Discovery kit and a new expansion board: B-WBA5M-WPAN
- Extended the implementation of the CMake and Makefile build generators taking into account the memory management tool (MMT) features:
- Single-core microcontrollers without Arm® TrustZone®(a), excluding STM32H7Rx/7Sx, or with disabled TrustZone®
- Dual-core microcontrollers without TrustZone® (such as in the STM32H7 series)
- Add the support of the memory management tool on STM32H7 dual-core and STM32WBA5Mxx microcontrollers
- Added the compare projects feature to make user able to differentiate between two STM32CubeMX project files across different microcontrollers and microprocessors.
- Implemented the loading of the firmware or applications code from the external memory (EXTMEMLOADER) using the OpenBootloader interface for STM32H7Rx/7Sx.
Main fixed issues in 6.13.0:
Refer to the STM32 microcontroller wiki at:
https://wiki.st.com/stm32mcu/wiki/Category:STM32CubeMX_errata
Known problems and limitations:
Refer to the STM32 microcontroller wiki at:
https://wiki.st.com/stm32mcu/wiki/Category:STM32CubeMX_errata
How to get STM32CubeMX 6.13.0:
- Under this link
- Or update your current installation of STM32CubeMX using: Help > Check for updates
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.