cancel
Showing results for 
Search instead for 
Did you mean: 

qt programing and stm32mp157d-dk1

Sharan
Senior II

hi

i am using stm32mp157d-dk1 and i have downloaded qt creator and i have created a simple hello world window now how to display it in the stm32mp157d-dk1?

 

how to set up cross compilation in order to deploy Qt projects directly from a host Linux machine to the embedded target using qtcreator.

1 ACCEPTED SOLUTION

Accepted Solutions
Sharan
Senior II

i hope i have got the steps right and for any of the steps bellow does it require internet                                                 1.cd <working directory path>/Distribution-Package

2.repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-6.1-yocto-mickledore-mpu-v24.06.26

3.repo sync

4. DISTRO=openstlinux-weston MACHINE=stm32mp15-disco source layers/meta-st/scripts/envsetup.sh

5.bitbake st-image-weston

6.bitbake st-image-weston -c populate_sdk

7. cd <Distribution Package installation directory>
8.git clone -b v1.0.0 https://github.com/STMicroelectronics/meta-st-x-linux-qt.git layers/meta-st/meta-st-x-linux-qt

9. git clone -b scarthgap https://github.com/meta-qt5/meta-qt5.git layers/meta-qt5

10. source layers/meta-st/scripts/envsetup.sh

11.bitbake-layers add-layer ../layers/meta-qt5 ../layers/meta-st/meta-st-x-linux-qt

12.bitbake st-image-qt

13.bitbake st-image-qt -c populate_sdk

14.execute "xxx.sh" script available in: build-openstlinuxweston-stm32mp15-disco/tmp-glibc/deploy/sdk

15.setup qt

View solution in original post

34 REPLIES 34
PPAGE.13
ST Employee

Duplicated:

https://community.st.com/t5/stm32-mpus-embedded-software-and/qt-creater-setup-for-stm32mp1/m-p/728333

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Sharan
Senior II

i was downloading distribution package ,while using this  command "repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-6.1-yocto-mickledore-mpu-v24.06.26" i am getting error as bellow

emertxe@ubuntu:~/STM32MPU/Distribution-Package$ repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-6.1-yocto-mickledore-mpu-v24.06.26


File "/home/emertxe/STM32MPU/Distribution-Package/.repo/repo/main.py", line 95
)
^
SyntaxError: invalid syntax

 

Hello @Sharan ,

I guess this is a repo tool issue, please have a look at : https://wiki.st.com/stm32mpu/wiki/PC_prerequisites.

(note: remove ".repo" directory if you do a new trail)

BR,

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Sharan
Senior II

yes i was able to solve the repo issue by changing the shebang line but now  bitbake st-image-weston requires  python 3.8.0 what to do

Sharan
Senior II

you had mentioned "If you get the SDK with Developper Package and X-LINUX-Qt SDK add-on, the installation automatically configures Qt creator with the MP1 kit." but for X-LINUX-QT is for stm32mp25x lines can u use that add on for stm32mp15x lines?

 

 

Hello @Sharan

X-LINUX-Qt will officially supports MP1x series in a few weeks.

But with the current delivery you can compile Distribution Package for "stm32mp15-disco" MACHINE.

Then when you run application on target, please use EGLFS configuration. In Wayland configuration you might face display synchronization we have fixed in the next coming delivery.

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Sharan
Senior II

https://barenakedembedded.com/how-to-set-up-stm32mp1-with-qt/                 

using this can i set up my stm with qt?

Hello @Sharan ,

no, please use official and updated documentation:

https://wiki.st.com/stm32mpu/wiki/X-LINUX-QT_Expansion_Package

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Sharan
Senior II

i am getting bitbake error please help me

 

 

 

NOTE: Fetching uninative binary shim http://downloads.yoctoproject.org/releases/uninative/4.3/x86_64-nativesdk-libc-4.3.tar.xz;sha256sum=1c35f09a75c4096749bbe1e009df4e3968cde151424062cf4aa3ed89db22b030 (will check PREMIRRORS first)
WARNING: Your host glibc version (2.39) is newer than that in uninative (2.38). Disabling uninative so that sstate is not corrupted.
Initialising tasks: 100% |###############################################################################################################################################| Time: 0:00:11
Sstate summary: Wanted 3246 Local 0 Mirrors 0 Missed 3246 Current 0 (0% match, 0% complete)
NOTE: Executing Tasks
ERROR: PermissionError: [Errno 1] Operation not permitted

During handling of the above exception, another exception occurred:

Traceback (most recent call last):
  File "/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/bitbake/bin/bitbake-worker", line 275, in child
    bb.utils.disable_network(uid, gid)
  File "/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/bitbake/lib/bb/utils.py", line 1693, in disable_network
    with open("/proc/self/uid_map", "w") as f:
PermissionError: [Errno 1] Operation not permitted

ERROR: Task (/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/meta/recipes-devtools/gcc/gcc-source_12.3.bb:do_rm_work) failed with exit code '1'
ERROR: PermissionError: [Errno 1] Operation not permitted

During handling of the above exception, another exception occurred:

Traceback (most recent call last):
  File "/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/bitbake/bin/bitbake-worker", line 275, in child
    bb.utils.disable_network(uid, gid)
  File "/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/bitbake/lib/bb/utils.py", line 1693, in disable_network
    with open("/proc/self/uid_map", "w") as f:
PermissionError: [Errno 1] Operation not permitted

ERROR: Task (/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/meta-st/meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp_6.1.bb:do_rm_work) failed with exit code '1'
NOTE: Tasks Summary: Attempted 6 tasks of which 0 didn't need to be rerun and 2 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 3 seconds

Summary: 2 tasks failed:
  /home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/meta/recipes-devtools/gcc/gcc-source_12.3.bb:do_rm_work
  /home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/meta-st/meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp_6.1.bb:do_rm_work
Summary: There was 1 WARNING message.
Summary: There were 2 ERROR messages, returning a non-zero exit code.