2024-10-06 11:59 PM - edited 2024-10-07 2:25 AM
hi
i am using stm32mp157d-dk1 and i have downloaded qt creator and i have created a simple hello world window now how to display it in the stm32mp157d-dk1?
how to set up cross compilation in order to deploy Qt projects directly from a host Linux machine to the embedded target using qtcreator.
Solved! Go to Solution.
2024-10-13 2:20 AM
i have installed the distribution package and followed the bellow steps
and what do do now to set up qt creator?
To install the X-LINUX-QT Distribution Package
cd <Distribution Package installation directory> git clone -b v1.0.0 https://github.com/STMicroelectronics/meta-st-x-linux-qt.git layers/meta-st/meta-st-x-linux-qt
git clone -b scarthgap https://github.com/meta-qt5/meta-qt5.git layers/meta-qt5
Source the build environment with the correct board and layers:
DISTRO=openstlinux-weston MACHINE=stm32mp2 BSP_DEPENDENCY="layers/meta-qt5 layers/meta-st/meta-st-x-linux-qt" source layers/meta-st/scripts/envsetup.sh
Add the layers to the Yocto environment:
cd <Distribution Package installation directory> source layers/meta-st/scripts/envsetup.sh bitbake-layers add-layer ../layers/meta-qt5 ../layers/meta-st/meta-st-x-linux-qt
and
2024-10-14 12:14 AM
I went with developer package as i was not able to do the distribution package
so the steps i followed for developer package was
i downloaded the MP1-DEV-x86 from st website
For x86_64 host architecture i Uncompressed the tarball file to get the SDK installation script. and Ran the SDK installation script.
for x-linux-qt developer package i downloded the below file(but my board is stm32mp157d-dk1)
i followed these steps
in the terminal i download qt creator using sudo apt install qtcreator and it installed (qt 5.15.13) and u had said Qt Creator will be configured automatically and you will get your MPU kit all set in Qt creator. but i cant find anything other than Qt 5.15.13(system)
2024-10-14 12:31 AM
The full MP1 X-LINUX-Qt support will be available in the coming weeks.
Distribution Package allows anyway user to compile with Qt libraries and run Qt application on MP1.
But for Qt creator MP1 kit configuration, you have to do it manually. Please refer to that post:
For MP2, the SDK-add on configures Qt creator kit automatically, but for MP1, the SDK-Addon is not yet delivered. Sorry of the inconvinience. It will be release soon.
Philippe.
2024-10-14 12:37 AM - edited 2024-10-14 12:39 AM
i am doing it manually it is showing no compiler can produce code for this qt version
2024-10-14 12:41 AM
Please look at the post I listed before, it will describe how to get the SDK and how to use it
(bitbake st-image-qt -c populate_sdk, ...)
2024-10-14 12:46 AM
it is showing like this when i run that
WARNING: Setscene task (/home/sharan/STM32MPU/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/meta/recipes-core/glibc/glibc_2.37.bb:do_populate_sysroot_setscene) failed with exit code '1' - real task will be run instead
NOTE: Tasks Summary: Attempted 496 tasks of which 494 didn't need to be rerun and 2 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 5 seconds
Summary: 2 tasks failed:
/home/sharan/STM32MPU/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/meta/recipes-kernel/linux-libc-headers/linux-libc-headers_6.1.bb:do_unpack
/home/sharan/STM32MPU/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/meta/recipes-kernel/linux-libc-headers/linux-libc-headers_6.1.bb:do_prepare_recipe_sysroot
Summary: There were 302 ERROR messages, returning a non-zero exit code.
2024-10-14 9:41 PM - edited 2024-10-15 1:28 AM
can someone please verify these steps please check the steps and correct me if i am wrong
steps to download distribution package
1.cd <working directory path>/Distribution-Package
2.repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-6.1-yocto-mickledore-mpu-v24.06.26
3.repo sync
4. DISTRO=openstlinux-weston MACHINE=<machine> source layers/meta-st/scripts/envsetup.s
5.bitbake st-image-weston
6. cd <Distribution Package installation directory>
7.git clone -b v1.0.0 https://github.com/STMicroelectronics/meta-st-x-linux-qt.git layers/meta-st/meta-st-x-linux-qt
8. git clone -b scarthgap https://github.com/meta-qt5/meta-qt5.git layers/meta-qt5
9. DISTRO=openstlinux-weston MACHINE=stm32mp2 BSP_DEPENDENCY="layers/meta-qt5 layers/meta-st/meta-st-x-linux-qt" source layers/meta-st/scripts/envsetup.sh
10.bitbake st-image-qt
11.bitbake st-image-qt -c populate_sdk
12.sdk generation refering to this doc https://wiki.st.com/stm32mpu/wiki/How_to_create_an_SDK_for_OpenSTLinux_distribution and using this command
bitbake -c populate_sdk st-image-weston
2024-10-15 1:57 AM
Hi Sharan,
So you should get these command sequence
4. DISTRO=openstlinux-weston MACHINE=stm32mp15-disco source layers/meta-st/scripts/envsetup.sh
7. git clone -b v1.0.0 https://github.com/STMicroelectronics/meta-st-x-linux-qt.git layers/meta-st/meta-st-x-linux-qt
8. git clone -b scarthgap https://github.com/meta-qt5/meta-qt5.git layers/meta-qt5
9.
bitbake-layers add-layer ../layers/meta-qt5 ../layers/meta-st/meta-st-x-linux-qt
9. DISTRO=openstlinux-weston MACHINE=stm32mp2 BSP_DEPENDENCY="layers/meta-qt5 layers/meta-st/meta-st-x-linux-qt" source layers/meta-st/scripts/envsetup.sh
10.bitbake st-image-qt
11.bitbake st-image-qt -c populate_sdk
2024-10-16 12:01 AM - edited 2024-10-16 12:39 AM
1)first question
after the 5th (that is bitbake st-image-weston) step do u have to execute this commad bitbake st-image-weston -c populate_sdk
2)second question
after the 11th step do we have to execute the bellow one ?
Then install the SDK: execute "xxx.sh" script available in: build-openstlinuxweston-stm32mp15-disco/tmp-glibc/deploy/sdk
3)third question
how many gb should i need to allocate for the above commands in virtual box and what version of qt creator should i need to install
4)does the above commands require internet?
2024-10-16 12:59 AM
"bitbake st-image-weston -c populate_sdk" command is necessary to generate the SDK .sh script.
This SDK .sh script (in build-openstlinuxweston-stm32mp15-disco/tmp-glibc/deploy/sdk) has to be executed.
This will create a SDK directory you will have to refer to in Qt creator.
Qt Creator 12.x.y can be used.