2021-12-02 01:22 PM
am getting things like Multiple Problems have occurred. Compacting Resource Model. Refreshing Workspace, Workbench Autosave Job.
An internal error occurred while showing an internal error.
It says look at the .log file. I have not found where that is on my Linux computer.
I am running workspace 1.5.1 it looks like the latest is 1.8. Should I just wipe out the STMCubeIDE and start over?
I think a java update for the IDE yesterday killed this. I remember seeing it say something about running out of mermory. My whole system is using 5.6 GB out of the 32 GB installed.
2021-12-02 01:41 PM
I looked in the project file and there are 270 files that end with .log.
I have a crash.log
/home/kip/STM32CubeIDE/workspace_1.5.1/Heidenhein-157-M4/external/mesa3d/src/freedreno/.gitlab-ci/reference/crash.log
But the forum will not let me upload it from its location because it will not let me look at a hidden directoty. (,getlab-ci)
I had to copy it to the desktop then upload from there.
2021-12-02 02:04 PM
There is a .log file.
It has a few lines.
Superblock has invalid MMP magic. Fix? yes
Pass 1: Checking inodes, blocks, and sizes
Pass 2: Checking directory structure
Pass 3: Checking directory connectivity
Pass 4: Checking reference counts
Pass 5: Checking group summary information
test_filesys: 11/128 files (0.0% non-contiguous), 19/512 blocks
Exit status is 0
But it was dated yesterday not today.