2019-12-12 02:06 AM
alex@NUC:~/Projects/stm32mp1/ecosystem/starter-package/stm32mp1-openstlinux-4.19-thud-mp1-19-10-09/images/stm32mp1$ STM32_Programmer_CLI -l usb -------------------------------------------------------------------
STM32CubeProgrammer v2.2.1
-------------------------------------------------------------------
===== DFU Interface =====
Total number of available STM32 device in DFU mode: 1
Device Index : USB1
USB Bus Number : 001
USB Address Number : 002
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
Serial number : 002900373338510534383330
Firmware version : 0x0110
Device ID : 0x0500
2019-12-12 02:11 AM
Hi @AMohr.1
This is a known issue in V2.2.1. Sorry for inconvenience.
Recommanded version is the V2.2.0.
Olivier
2019-12-12 02:13 AM
Alternatively, it should work with v2.2.1 using the GUI instead of command line.