cancel
Showing results for 
Search instead for 
Did you mean: 

Create Custom SDK Error

FarukSozuer
Associate III

Hello everyone,

I got a yocto build from scratch using yocto/open-embedded/meta-st-stm32mp. Everything is smooth. I can root the kernel while standing. I can establish an ssh connection. Everything is perfect.

But I want to create an SDK after the kernel compilation I received. In the next step, I will integrate the SDK I created into cubeide and start developing code. But when I say "bitbake -c populate_sdk core-image-minimal" I get the following error. I've been struggling with this error all day and couldn't solve it. Does anyone have an idea?

Screenshot from 2024-06-25 23-50-50.png

 

Sincelery

1 ACCEPTED SOLUTION
1 REPLY 1