cancel
Showing results for 
Search instead for 
Did you mean: 

Wlan0: Unsupported driver ‘nl80211’

SigmaPrime
Senior

I am working with Buildroot, to flash an image on my STM32MP157C-DK2 I wanted to have Wi-Fi working it but I got this error:

Code:

Copy to clipboard

Successfully initialized wpa_supplicant

nl80211: 'nl80211' generic netlink not found

Failed to initialize driver 'nl80211'

wlan0: Unsupported driver 'nl80211'

FAIL

I configure the interfaces and wpa_supplicant.conf files correctly normally. I don’t know wthat that means but my configuration in the menuconfig and linux-menuconfig is right (I think). Does it maybe have something to do with my target machine (the STM in this case) ?

Every Kind of Help is appreciated since I am a newby in Embedded Linux

p.s I don’t know why but it seems like the Wifi Bluetooth Card is Murata-LBEE5KL1DX-883. Maybe my Kernel configuration does not support it

I linked both Kernel and System Configuration

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @SigmaPrime​ ,

I guess @Lukas Brückner​ gives you useful hint about the same problem in your other post :

https://community.st.com/s/question/0D53W00000M9LPsSAN/mpu-nteraction-with-a-endpointrest-through-wifi

Do you confirm ?

Thx

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.